Tool/software: Linux
Hello,
I want ip packets to be sent between the two interfaces on the evm board.
For example, set eth0 to 192.168.1.2 and eth1 to 192.168.2.2. Each interface is connected to a host.
Assign the IP address of 192.168.1.3 to the host connected to eth0, and the IP of 192.168.2.3 to the host connected to eth1.
At this time, how do I configure the host connected to eth0 to ping the host connected to eth1?
BR,
Namki Lee.