Part Number: TMS320C6678
Hello,
There are three c6678 on a board and I assembled two board.
Three DSP are successfully boot on board #1 but on board #2 only two DSP's booting are successful.
I checked input voltage and clock for boot failed DSP on board #2 and found no abnormal state.
I wrote down my debug result on board #2 below:
1> I can connect and write down binary code to DSP by debugger when no boot mode. When no boot mode, I can connect all of three DSPs without error.
2> Then I changed boot mode to EMIF16 boot mode then power down.
3> After power on, one DSP's boot is failed. The CS signal of NOR flash is changed for a short time after power on, so I belived that DSP's boot mode is well set.
4> When EMIF16 boot mode, I can connect target to two DSPs which boot are successful without any error but I can not connect target to boot failed DSP. When I tried to connect to boot failed DSP by debugger, I faced error message - 'Error connecting to the target(Error - 1143 @ 0x0)' or ''Error connecting to the target(Error - 1144 @ 0x0)'
I need to know what difference there are between boot failed DSP and boot succeed DSP.
-> On no bootmode, I can connect target to all three DSPs by debugger.
-> On EMIF16 bootmode, I can connect target by debugger only two DSPs which are successfully boot.