Part Number: AM5728
Tool/software: Linux
Hi,
I'm using AM572x custom board
How to use QSPI & MCSPI Flash together in U-BOOT
I want to use SPI & Quad SPI together.
But, I cannot use it. When I use "u-boot sf probe command"...... it doesn't work.
=> sf probe 0:0
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB, mapped at 5c000000
=> sf probe 0:1
SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000
Failed to initialize SPI flash at 0:1 (error -93)
=> sf probe 0:2
SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000
Failed to initialize SPI flash at 0:2 (error -93)
=> sf probe 0:3
SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000
Failed to initialize SPI flash at 0:3 (error -93)
=> sf probe 0:4
SF: Detected S25FL256S_64K with page size 256 Bytes, erase size 64 KiB, total 32 MiB, mapped at 5c000000
=> sf probe 1:0
Invalid bus 1 (err=-19)
Failed to initialize SPI flash at 1:0 (error -19)
=> sf probe 1:1
Invalid bus 1 (err=-19)
Failed to initialize SPI flash at 1:1 (error -19)
=> sf probe 1:2
Invalid bus 1 (err=-19)
Failed to initialize SPI flash at 1:2 (error -19)
=> sf probe 1:3
Invalid bus 1 (err=-19)
Failed to initialize SPI flash at 1:3 (error -19)
=> sf probe 2:0
Invalid bus 2 (err=-19)
Failed to initialize SPI flash at 2:0 (error -19)
=> sf probe 2:1
Invalid bus 2 (err=-19)
Failed to initialize SPI flash at 2:1 (error -19)
=> sf probe 2:2
Invalid bus 2 (err=-19)
Failed to initialize SPI flash at 2:2 (error -19)
I want to show your opinion.
Thank you.
Pinmux U-Boot
QSPI:
{GPMC_A13, (M1 | PIN_INPUT_PULLDOWN | MANUAL_MODE)}, /* gpmc_a13.qspi1_rtclk */
{GPMC_A14, (M1 | PIN_INPUT_PULLUP | MANUAL_MODE)}, /* gpmc_a14.qspi1_d3 */
{GPMC_A15, (M1 | PIN_INPUT_PULLUP | MANUAL_MODE)}, /* gpmc_a15.qspi1_d2 */
{GPMC_A16, (M1 | PIN_INPUT_PULLDOWN | MANUAL_MODE)}, /* gpmc_a16.qspi1_d0 */
{GPMC_A17, (M1 | PIN_INPUT_PULLDOWN | MANUAL_MODE)}, /* gpmc_a17.qspi1_d1 */
{GPMC_A18, (M1 | PIN_INPUT_PULLDOWN | MANUAL_MODE)}, /* gpmc_a18.qspi1_sclk */
SPI1:
{SPI1_SCLK, (M0 | PIN_INPUT_PULLDOWN | MANUAL_MODE)}, /* gpmc_a18.qspi1_sclk */
{SPI1_D1, (M0 | PIN_INPUT_PULLDOWN)}, /* spi1_d1.gpio7_8 */
{SPI1_D0, (M0 | PIN_INPUT_PULLDOWN)}, /* spi1_d0.gpio7_9 */
{SPI1_CS0, (M0 | PIN_INPUT_PULLDOWN)}, /* spi1_cs0.gpio7_10 */
U-Boot dts file (am572x-idk.dts)
&qspi {
status = "okay";
spi-max-frequency = <76800000>;
m25p80@0 {
compatible = "s25fl256s1","spi-flash";
spi-max-frequency = <76800000>;
reg = <0>;
spi-tx-bus-width = <1>;
spi-rx-bus-width = <4>;
#address-cells = <1>;
#size-cells = <1>;
};
};
&mcspi1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&mcspi1_pins>;
m25p80@1{
compatible = "N25Q256A","spi-flash";
reg = <0>;
};
};
My Development Environment
Host PC OS: Ubuntu 16.04 linux 64bit
AM5728 SDK: u-boot-2016.05 / linux-rt-4.4.19
AM5728 SDK Ver: ti-processor-sdk-linux-rt-am57xx-evm-03.01.00.06
IPC: ipc_3_43_02_04
XDC: xdctools_3_32_00_06_core
Thanks and best regards.
John.