This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J6EVM5777: OpenCV unit tests on J6 EVM

Part Number: J6EVM5777

Hi all,

I'm testing opencv base on PSDKLA 3.02. (prebuilt image) 

First, is the command describe in the wiki correctly? After source setupEnv.sh, I need execute "ifconfig"??? 

I followed the step describe in below link.


but it seems stuck.... I wait a few hours...

  

My question are

1. Can this unit tests run on DRA7xx ??

2. Do I need to modify OPENCV_OPENCL_DEVICE variable which defined in the setupEnv.sh?

3. Is there any other steps should be done?

Thanks in advanced.

AC