Tool/software: Linux
Hi :
I using J6eco evm board with Qt5 app.
My bsp version : ti-glsdk_dra7xx-evm_7_04_00_03 with yocto-layers
now I follow the guide of http://processors.wiki.ti.com/index.php/DRA7xx_QT5_on_GLSDK ,
and can't install success.
1. Updating the top level config file:
file: configs/glsdk/glsdk-7.04.00.03-config.txt
# meta-qt5,git://github.com/meta-qt5/meta-qt5.git,master,f728a6b8a50e12d7da9b70c8093c484d48b33ca8,layers=
# meta-qt5,git://github.com/meta-qt5/meta-qt5.git,daisy,dc277b5a52e3da6b7b50c9f5f2e185f841788e33,layers=
meta-qt5,git://github.com/meta-qt5/meta-qt5.git,master,48ebff679e5dc084d395b861a1fc4cb21790d51b,layers=
2.Updating the meta-glsdk
file:sources/meta-glsdk/conf/distro/arago.conf
add to the end
QT_PROVIDER ?= "qt5" # Configure Qt5 flags (GLES is still required for qtdeclarative and qtwebkit) PACKAGECONFIG_GL_pn-qtbase = "gles2 linuxfb" PACKAGECONFIG_DISTRO_pn-qtbase = "icu examples" # Configure gstreamer-0.10.x as a dependency instead of gstreamer-1.x PACKAGECONFIG_pn-qtwebkit = "gstreamer qtlocation qtmultimedia qtsensors"
file :sources/meta-glsdk/meta-glsdk/meta-arago-distro/recipes-core/packagegroups/packagegroup-arago-glsdk-multimedia.bb
add this.
packagegroup-arago-tisdk-qte \
3. Redo the GLSDK Yocto build
NOTE: Preparing runqueue
WARNING: /home/zhan/ti-glsdk_dra7xx-evm_7_04_00_03/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-multimedia/gst-plugins-ti/gstreamer1.0-plugins-ducati_git.bb.do_configure is tainted from a forced run
WARNING: /home/zhan/ti-glsdk_dra7xx-evm_7_04_00_03/yocto-layers/sources/meta-arago/meta-arago-extras/recipes-multimedia/gst-plugins-ti/gstreamer1.0-plugins-vpe_git.bb.do_configure is tainted from a forced run
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL download.qt-project.org/.../qtbase-opensource-src-5.4.1.tar.xz, attempting MIRRORS if available
WARNING: Failed to fetch URL download.qt-project.org/.../qtdeclarative-opensource-src-5.4.1.tar.xz, attempting MIRRORS if available
ERROR: Fetcher failure: Fetch command failed with exit code 8, output:
download.qt.io/.../qtbase-opensource-src-5.4.1.tar.xz:
2017-04-20 00:10:15 ERROR 404: Not Found.
ERROR: Function failed: Fetcher failure for URL: 'download.qt-project.org/.../qtbase-opensource-src-5.4.1.tar.xz'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/zhan/ti-glsdk_dra7xx-evm_7_04_00_03/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/qtbase-native/5.4.1-r0/temp/log.do_fetch.7145
ERROR: Task 4077 (/home/zhan/ti-glsdk_dra7xx-evm_7_04_00_03/yocto-layers/sources/meta-qt5/recipes-qt/qt5/qtbase-native_5.4.1.bb, do_fetch) failed with exit code '1'
WARNING: Failed to fetch URL download.qt-project.org/.../qtbase-opensource-src-5.4.1.tar.xz, attempting MIRRORS if available
Waiting for 3 running tasks to finish:
0: qtbase-5.4.1-r0-arago8 do_fetch (pid 7146)
1: qtdeclarative-5.4.1-r0 do_fetch (pid 7149)
2: qt3d-5.4.1+gitAUTOINC+8a9723d742-r0 do_fetch (pid 7165)
. . . . . .
what can i do for the bsp and Qt5?
Thanks .