Hello,
As per above description is seems that a interrupt ca be is used for IPC using CORTEXM4_CTRL_REG.
What will be the interrupt signal that will be generated ?
Whether this interrupt needs to be enabled/disabled ? Then from where ?
Crossbar configuration required ? which interrupt signal to use with crossbar ?
Is this an interrupt or a dedicated exception ?
The description says that the priority for the interrupt is configurable but I could not find any interrupt signal associated with this interrupt ?
Regards,
Yuvraj