This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H264 decoder for DM6467 hangs when exit

Hi, guys, 

 

We are using H264DEC for DM6467 ( BP/MP/HP, version: 01.10.04.00, all other tools are coming from DVSDK  3.10.00.11), and we encounter a problem: 

 

When we send a SIGKILL or SIGINT (kill -9, or CTRL+C) to the `encodedecode` demo,  the demo would hang there, and the process becomes a Zombie.  we try to trace which call hangs, and found its VIDDEC2_process();

 

I am wondering if this is a codec problem or CE problem, but any suggestions would be highly appreciated.  Thanks. 

 

Regards

 

Wang Ning

 

FYI: 

 

CE: 2.25.01.06

 

BIOS: 5.41.00.06

 

XDC: 3.16.01.27