Part Number: AM5728
Hi all,
I encountered some problems when I used DCAN.
I was able to set the bitrate, but when I tried to turn on the device, the following error:
root@am57xx-evm:~# canconfig can0 bitrate 50000 ctrlmode triple-sampling on
can0 bitrate: 50000, sample-point: 0.875
can0 ctrlmode: loopback[OFF], listen-only[OFF], tripple-sampling[ON],one-shot[OF
F], berr-reporting[OFF]
root@am57xx-evm:~# canconfig can0 start
[ 1149.882464] net can0: c_can_hw_raminit_wait_syscon: time out
[ 1149.888401] c_can_platform 4ae3c000.can can0: setting BTR=1c18 BRPE=0000
can0 state: ERROR-ACTIVE
This is dmesg and the driver loads the print:
root@am57xx-evm:~# dmesg | grep can
[ 6.415792] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 6.658759] pinctrl-single 4a003400.pinmux: could not add functions for dcan1
_pins_default 14288x
[ 6.692822] c_can_platform 4ae3c000.can: c_can_platform device registered (re
gs=fce3c000, irq=356)
[ 1149.882464] net can0: c_can_hw_raminit_wait_syscon: time out
[ 1149.888401] c_can_platform 4ae3c000.can can0: setting BTR=1c18 BRPE=0000
root@am57xx-evm:~# lsmod | grep can
c_can_platform 6604 0
c_can 9462 1 c_can_platform
can_dev 12292 1 c_can
I can find the CAN0 device after executing the 'canconfig can0 start' command
root@am57xx-evm:~# ifconfig
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
-00
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:100
This is some information when I execute the 'cansequence' command
root@am57xx-evm:~# cansequence can0
interface = can0, family = 29, type = 3, proto = 1
[ 185.975735] can: controller area network core (rev 20120528 abi 9)
[ 185.982345] NET: Registered protocol family 29
[ 185.991247] can: raw protocol (rev 20120528)
^C
root@am57xx-evm:~# cat /proc/net/can/stats
1286933 transmitted frames (TXF)
3 received frames (RXF)
0 matched frames (RXMF)
0 % total match ratio (RXMR)
0 frames/s total tx rate (TXR)
0 frames/s total rx rate (RXR)
0 % current match ratio (CRXMR)
0 frames/s current tx rate (CTXR)
0 frames/s current rx rate (CRXR)
0 % max match ratio (MRXMR)
481206 frames/s max tx rate (MTXR)
3 frames/s max rx rate (MRXR)
0 current receive list entries (CRCV)
0 maximum receive list entries (MRCV)
root@am57xx-evm:~# lsmod | grep can
can_raw 6589 1
can 29605 1 can_raw
c_can_platform 6604 0
c_can 9462 1 c_can_platform
can_dev 12292 1 c_can
root@am57xx-evm:~# dmesg | grep can
[ 5.981282] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[ 6.187731] pinctrl-single 4a003400.pinmux: could not add functions for dcan1
_pins_default 14288x
[ 6.203728] c_can_platform 4ae3c000.can: c_can_platform device registered (re
gs=fce3c000, irq=356)
[ 129.752423] net can0: c_can_hw_raminit_wait_syscon: time out
[ 129.758349] c_can_platform 4ae3c000.can can0: setting BTR=1c18 BRPE=0000
[ 185.975735] can: controller area network core (rev 20120528 abi 9)
[ 185.991247] can: raw protocol (rev 20120528)
I tested using two boards to connect:
I've ever sent a post:
https://e2e.ti.com/support/arm/sitara_arm/f/791/p/562088/2060062#pi316653=1
According to your proposal to change the hardware can be used after.
Now my hardware and software and the same as before, but prompted me to pinmux problems,this is my pinmux.
&dra7_pmx_core {
dcan1_pins_default: dcan1_pins_default {
pinctrl-single,pins = <
0x37d0 (PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* dcan1_tx */
0x37d4 (PIN_INPUT_PULLUP | MUX_MODE0) /* dcan1_rx */
>;
};
};
&dcan1 {
status = "okay";
pinctrl-names = "default";
pinctrl-0 = <&dcan1_pins_default>;
};
Hope you can help me solve this problem.
Thanks