Part Number: PROCESSOR-SDK-AM57X
Tool/software: Linux
Hi!
I am currently testing IPC between Linux and the C66x DSP Coprocessor on the AM57xx SOC.
I need some advice regarding the remoteproc subsystem in the Linux Kernel:
Here is a code snippet of the rsc_table_vayu_dsp.h file, which I am using for my tests:
{
TYPE_CARVEOUT,
DSP_MEM_TEXT, 0,
DSP_MEM_TEXT_SIZE, 0, 0, "DSP_MEM_TEXT",
},
{
TYPE_CARVEOUT,
DSP_MEM_DATA, 0,
DSP_MEM_DATA_SIZE, 0, 0, "DSP_MEM_DATA",
},
{
TYPE_CARVEOUT,
DSP_MEM_HEAP, 0,
DSP_MEM_HEAP_SIZE, 0, 0, "DSP_MEM_HEAP",
},
If I understand it correctly, then the whole generated Code of the DSP will be mapped to the Main Memory of the AM57xx SOC, using the DSP MMU. Is that correct?
The linker.cmd file confirms this, as all sections are mapped to some kind of virtual address and not to the internal memory which is located at 0x800000:
MEMORY
{
L2SRAM (RWX) : org = 0x800000, len = 0x40000
OCMC_RAM1 (RWX) : org = 0x40300000, len = 0x80000
OCMC_RAM2 (RWX) : org = 0x40400000, len = 0x100000
OCMC_RAM3 (RWX) : org = 0x40500000, len = 0x100000
EXT_CODE (RWX) : org = 0x95000000, len = 0x100000
EXT_DATA (RW) : org = 0x95100000, len = 0x100000
EXT_HEAP (RW) : org = 0x95200000, len = 0x300000
TRACE_BUF (RW) : org = 0x9f000000, len = 0x60000
EXC_DATA (RW) : org = 0x9f060000, len = 0x10000
PM_DATA (RWX) : org = 0x9f070000, len = 0x20000
}
SECTIONS
{
.text: load >> EXT_CODE
.ti.decompress: load > EXT_CODE
.stack: load > EXT_DATA
GROUP: load > EXT_DATA
{
.bss:
.neardata:
.rodata:
}
.cinit: load > EXT_DATA
.pinit: load >> EXT_DATA
.init_array: load > EXT_DATA
.const: load >> EXT_DATA
.data: load >> EXT_DATA
.fardata: load >> EXT_DATA
.switch: load >> EXT_DATA
.sysmem: load > EXT_DATA
.far: load >> EXT_DATA
.args: load > EXT_DATA align = 0x4, fill = 0 {_argsize = 0x64; }
.cio: load >> EXT_DATA
.ti.handler_table: load > EXT_DATA
.c6xabi.exidx: load > EXT_DATA
.c6xabi.extab: load >> EXT_DATA
.tracebuf: load > TRACE_BUF
.errorbuf: load > EXC_DATA
.vecs: load > EXT_CODE
.resource_table: load > 0x95000000, type = NOINIT
xdc.meta: load > EXT_DATA, type = COPY
}
Now the question: What do I need to do if I want to use the IPC example as it is, but using the dedicated internal memory of the DSP?
I guess I need to modify the linker.cmd file to map all sections to L2SRAM and then remove all DSP_MEM_TEXT, DSP_MEM_DATA and DSP_MEM_HEAP from the resource table. Is that correct?
Just out of curiosity: What happens if I change the linker.cmd file to use the internal L2SRAM and also add the L2SRAM addresses as carveouts in the resource table?
From the remoteproc driver perspective it looks like the elf loader would place the DSP firmware into the correct physical L2SRAM location, however also the MMU would then be configured to map the address 0x800000 to the main memory. What would be the behavior then? Is it even possible to mmu-map the address 0x800000 to the main memory?
Thanks for your answer!
Regards,
Franz