Tool/software: TI-RTOS
CCS Version: 7.1.0.00016
sys/bios Version: bios_6_50_01_12
I have one Hwi and two tasks, task1 and task2.
The priority of task1 is higher than task2. now, I want to achieve the function as follows:
Run Task1 after Hwi, then run Task2 after Task1 finished, and then go to Idle loop and wait for Hwi again after task2 finished.
The time between two Hwi is 64ms, and task1 if about 35ms, and task2 is about 10ms.
What can I do to achieve the function?
I have tried to post an event in Hwi to run task1, and post a semaphore to run task2 at the end of task1. but it didn't worked as what I expected.