This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2H14:Error in tftp server



Hi every one,

I want to fetch kernel from tftp server. I configure tftp server but when I write this commands:

  • setenv serverip <your tftp server IP set in the tftp SW>
  • setenv name_uboot <the actual entire .gph file name>
  • saveenv

every thing is ok but when I write this:

  • run get_uboot_net

it has an error like below:

what should I do to fix this error?

for <your tftp server IP set in the tftp SW> I used this IP which the modem is showing, is it right to use this IP?

Best regaeds,

Matin

  • Hi Matin,

    for <your tftp server IP set in the tftp SW> I used this IP which the modem is showing, is it right to use this IP?


    You need to use the IP of your host pc.
    You also need to make sure that host PC and the device belong to the same network and both are configured to use either static ip or DHCP (host pc is a server and your board is connected to it and gets ip from the dhcp server).

    Best Regards,
    Yordan