Tool/software: Linux
I hope this is the correct area for a problem I have regarding flashing and reading the u-boot env area to/from nand flash. Here is the sequence - any help would be appreciated
1. I Use u-boot's mkenvimage to generate a binary data file from a text file e.g ./mkenvimage -s 8192 -o env.bin env.txt
2. The environment variables are defined to go onto partition 5 so /etc/fw_env.config has this defined as follows:
MTD Device Name Device Offset Env. size Flash Sector Size Number of sectors
/dev/mtd5 0x0000 0x2000 0x20000 1
3. In Linux (SD card), write env.bin to nand flash as follows:
/usr/sbin/flash_erase /dev/mtd5 0 0
/usr/sbin/nandwrite -p /dev/mtd5 env.bin
All of this succeeds.
When I then try to boot from nand flash I get the following error:
when u-boot reads the env area.
Error: Bad compare! failed
..and proceeds to use the default environment.
It seems that it is failing because the calculated ecc differs fro the read ecc.
My question is, how is the ecc generated and where do I put a valid ecc count for my env.bin so that
the environment area is read correctly by u-boot.
Regards,
A Hart