Part Number: TMS320C6748
Other Parts Discussed in Thread: TLV320AIC3106
Dear forum
I need to use SPI for control a device; this device, as tipical, have the SS input pin.
Question are:
1)Connect to SS, i need to use the SPI0_ENA or the SPI0_CS[0] of the C6748 ?
2) In case SPI0_ENA is not necessary, can I use it as EPWM0B ...the PWM genrator ?
3)The PWM will generate a square wave 50% as input clock for a Audio Codec. It is good for this purpose
or the square quality is low for such application ?
Many Thanks
Roberto