This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/66AK2E05: Error in loading Linux through CCS

Part Number: 66AK2E05


Tool/software: Linux

Hi


i was trying to load linux kernel into the keystone kit via the method explained in the following link http://processors.wiki.ti.com/index.php/MCSDK_UG_Chapter_Exploring#Loading_and_Running_Linux_Kernel_on_EVM

i ended up with two errors

  1. arm_A15_0: Data verification failed at address 0xc5f0000
    arm_A15_0: Unable to terminate memory download: NULL buffer pointer at 0x3aa4- this error comes when i try to load the boot monitor. the uboot still runs normally and can be accessed via the serial port.
  2. the 2nd error is that when i run the kernel script (loadlin-evm-kern.js) it loads the memory smoothly when working on uImage-keystone-evm.bin but when i starts to load the tisdk-rootfs-k2e-evm.tar.gz it takes forever to load and when it reaches 50% it starts to go into negative values as can be seen in the picture below (-42%)

and help on how to fix this issue would be appreciated !!

regards

Hannan