Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3354
Tool/software: Linux
Hi all,
We have custom board with AM335x and SDK7 used for development. There are two USB host ports available in our design for connecting gadget devices. The problem we have observed is USB device not responding some time when plug it. This issue happen only when two ports are using ex. USB port1 connected with Pen drive already and connecting USB keyboard on second port. This issue occurs randomly when try to connect the keyboard device.
Have applied patches from following link but no luck,

Can any one help on this?
Thanks -Durai