This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: Debian packages for NAND

Part Number: PROCESSOR-SDK-AM335X

Tool/software: Linux

Hi,

I am using 1 GB NAND flash to boot-up the board which is based on AM335X SOM.

Now i have 2GB NAND flash,what are the required chages that i have to do.Because 1 GB sector size(2K) and 2GB sector size(4K) is different.

I am using yocto build system.

Is it possible to do common set of Debian packages for both 1GB and 2GB SOMs to make the packages upgrade process same for both the SOMs ??

Thanks in Advance.