hi everyone
i'm using VC5509 evalution board. i dont have xds510emu. i'm using ccs 3.3. i have a examples codes. i want know how to convert .bin file. i'm going to boot from usb. so can any one tel how to convert from .out file to .bin file. tel me the procedure. because i tried lots but i couldnt create. i used in cmd window hex55.exe -boot -v5510:2 -serial8 -reg_config 0x1c00,0x2180 -b -o <i file> <.o file>. after i created i tried to load via usb using USBIOAPP demo driver sw. but the processor will not boot. i dont know what eror. so pls send the procedure. i have changed boot mode option also.
thanks in advance