Part Number: DRA750
Other Parts Discussed in Thread: DRA752
Tool/software: Linux
We have custom daughter board + custom DRA752 CPU module board with uboot 2014.07 in glsdk 7.03.00.00.3 , but some our CPU modules which filter out by our MP line are bad.
Because those CPU modules can not boot up successfully , stucking in "starting kernel ..." during boot up, the log as below:
U-Boot 2014.07 (Apr 26 2017 - 16:16:36) CPU : DRA752-GP ES2.0 Board: DRA7xx I2C: ready DRAM: 2 GiB MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1, OMAP SD/MMC: 2 Using default environment serial# not set, setting... SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). SCSI: Net: Phy not found cpsw Hit any key to stop autoboot: 0 J6 ... Card did not respond to voltage select! Card did not respond to voltage select! switch to partitions #0, OK mmc1(part 0) is current device SD/MMC found on device 1 reading j6_uenv.txt 206 bytes read in 3 ms (66.4 KiB/s) Loaded environment from j6_uenv.txt Importing environment from mmc1 ... 5178640 bytes read in 121 ms (40.8 MiB/s) 101700 bytes read in 8 ms (12.1 MiB/s) Booting from mmc1 ... Kernel image @ 0x82000000 [ 0x000000 - 0x4f0510 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffe4000, end 8ffffd43 ... OK Starting kernel ...
Could you give us some direction to debug it ? ( it should be h/w issue , but we want to know which part is NG )
BTW, I have increased debug level (loglevel=8) in the j6_uenv.txt.
Best Regards,
Bowei Ren