This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: Can't get the wlan quality from /proc/net/wireless on Kernel 3.14 + wl18xx R8.6_SP1

Part Number: PROCESSOR-SDK-AM335X


Tool/software: Linux

Hi All,

Our system is based on the TI_SDK am335x-evm-01.00.00.03 + wilink driver R8.6_SP1.
(linux kernel 3.14)

We encounter a problem about wifi driver: there is no value in /proc/net/wireless.

We following the below steps to setup our system:
1. build image from TI_SDK am335x-evm-01.00.00.03 and install on the sd-card
2. build wifi driver and install to sd-card (update to R8.6_SP1,following this page:
processors.wiki.ti.com/.../WL18xx_System_Build_Scripts)

We want to know why it's empty in the /proc/net/wireless. Besides,
the iwlist can't use in our system either.

root@1646I3000058:/opt/sensors# cat /proc/net/wireless
Inter-| sta-|   Quality        |   Discarded packets               | Missed | WE
 face | tus | link level noise |  nwid  crypt   frag  retry   misc | beacon | 22
 
 
root@1646I3000058:/opt/sensors# iwlist wlan0 scan
wlan0     Interface doesn't support scanning.

root@1646I3000058:/opt/sensors# dmesg | grep wlcore
[    8.306570] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[    8.412364] wlcore: loaded
[    8.412418] wlcore: driver version: R8.6_SP1
[   15.315733] (stk) :ldisc_install = 1<6>[   15.600097] wlcore: PHY firmware version: Rev 8.2.0.0.233
[   15.647601] wlcore: firmware booted (Rev 8.9.0.1.55)
[   25.028840] wlcore: Association completed.
[  113.117680] wlcore: down
[  113.606835] wlcore: PHY firmware version: Rev 8.2.0.0.233
[  113.654443] wlcore: firmware booted (Rev 8.9.0.1.55)
[  186.883734] wlcore: Association completed.
[ 2180.252107] wlcore: down
[ 2181.370754] wlcore: PHY firmware version: Rev 8.2.0.0.233
[ 2181.417517] wlcore: firmware booted (Rev 8.9.0.1.55)
[ 2182.356583] wlcore: Association completed.
root@1646I3000058:/opt/sensors#

root@1646I3000058:/opt/sensors# iw wlan0 scan
BSS f4:7f:35:5e:8b:60(on wlan0) -- associated
        TSF: 2261873543407 usec (26d, 04:17:53)
        freq: 2462
        beacon interval: 102 TUs
        capability: ESS Privacy ShortPreamble ShortSlotTime RadioMeasure (0x1431)
        signal: -70.00 dBm
        last seen: 10 ms ago
        Information elements from Probe Response frame:
        SSID: Delta-Office
        Supported rates: 1.0* 2.0* 5.5* 6.0 9.0 11.0* 12.0 18.0
        DS Parameter set: channel 11
        Country: TW     Environment: Indoor/Outdoor
                Channels [1 - 11] @ 30 dBm
        BSS Load:
                 * station count: 7
                 * channel utilisation: 192/255
                 * available admission capacity: 23437 [*32us]
        ERP: Use_Protection
        HT capabilities:
                Capabilities: 0x182c
                        HT20
                        SM Power Save disabled
                        RX HT20 SGI
                        No RX STBC
                        Max AMSDU length: 7935 bytes
                        DSSS/CCK HT40
                Maximum RX AMPDU length 65535 bytes (exponent: 0x003)
                Minimum RX AMPDU time spacing: 8 usec (0x06)
                HT RX MCS rate indexes supported: 0-15
                HT TX MCS rate indexes are undefined
        RSN:     * Version: 1
                 * Group cipher: CCMP
                 * Pairwise ciphers: CCMP




Can anyone give us some idea about this issue?



thanks,
Jacob