Part Number: XTCIEVMK2LX
Other Parts Discussed in Thread: RFSDK, 66AK2L06
Tool/software: TI-RTOS
Hi,
I am using CCS 7.1.0.00016 and a TCIEVMK2LX evaluation board.
I want to use the FMC connector to read and write signals. It seems I need to use the Digital Front End for that. I imported the project "dfeUnitK2LC66TestProject", hoping that I would understand which functions to use in CCSv7.
However, this example is way too complex. Would it be possible for you to provide the simplest way to write "1" on the pin called JESD0_TXP_FMC1 ? That would be a great help.
Since I want the signal to go directly to the DSP, the DFE signal processing blocks should be bypassed. Thus I would also like to know how to use the bypass feature.
I already managed to use the GPDAC pins using the FPGA, but this is too slow for me.
Thanks in advance,
Matthias