This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/PROCESSOR-SDK-AM335X: TFTP boot on ICE board

Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: TMDSICE3359, AM3359

Tool/software: Linux

Hello,

I'm trying to get my TMDSICE3359 development board booting using TFTP.  I'm using the create-sdcard.sh script included in the processor SDK package to create the SD card to boot from.

Will the pre-built binaries used in the create-sdcard.sh script work correctly on a TMDSICE3359 development board?  I'm not able to download kernel images using TFTP.  I keep seeing messages from u-boot saying it's broadcasting BOOTP messages, but never see them being sent (when I watch with Wireshark).

The TMDSICE3359 uses a different PHY than other TI boards that use the AM3359.  Not sure if that has anything to do with it or not...

Any help would be greatly appreciated.