This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: LCD issues

Part Number: AM3352

Tool/software: Linux

Hi,

We are ported new sdk based on kernel 4.4.12 but facing issue related to brightness of LCD.

Before that our product was running on kernel 3.2.0 and now we have ported to 4.4.12. But with this new kernel version, brightness of LCD is changing any time even on run time or start up time.

It has 320x280 dimensions and working at 6.5 MHz frequency. Brightness control is based on pwm, nut we are keeping it constant at 90% duty cycle.

We have also verified that pwm/ecap0 pin as gpio to keep brightness constant, but issue is still same.  Platform data provided in board file of older kernel and dts file of new kernel is identical.

So, why this is happening.

Best Regards

Rohit Khatri