Part Number: AM3358
Test environment for modular AM3358 board that can be powered up with 1.8V or 3.3V on each of the VDDSHV individually may require powering those rails after the TPS65217C powers all the other power supplies to the AM3358 (including VDDS). Is there a potential to damage the AM3358 if VDDSHV power supplies are powered UP AFTER VDD_CORE and VDD_MPU? Is there a potential to damage the AM3358 if VDDSHV power supplies are powered DOWN BEFORE VDD_CORE and VDD_MPU?