Part Number: TMDXIDK5728
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
There appears to be something else configuring the resource table for DSP2 trying to use a custom resource table.
DSP1 works after installing it on the target idkAM5728 board. However DSP2 will not install. These messages are shown after the command use to install DSP2,
-----------------------------------------------
cd /lib/firmware
rm dra7-dsp2-fw.xe66
ln -s /lib/firmware/ipc/ipcm/server_dsp2_mod8.xe66 dra7-dsp2-fw.xe66
cd /sys/bus/platform/drivers/omap-rproc
echo 41000000.dsp > unbind
[24952.221267] omap_hwmod: mmu1_dsp2: _wait_target_disable failed
[24952.234417] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
[24952.240308] remoteproc3: stopped remote processor 41000000.dsp
[24952.247751] remoteproc3: releasing 41000000.dsp
echo 41000000.dsp > bind
[24999.808025] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
[24999.815857] remoteproc3: 41000000.dsp is available
[24999.820767] remoteproc3: Note: remoteproc is still under development and considered experimental.
[24999.829767] remoteproc3: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[24999.847427] remoteproc3: powering up 41000000.dsp
root@am57xx-evm:/sys/bus/platform/drivers/omap-rproc# [24999.852682] remoteproc3: Booting fw image dra7-dsp2-fw.xe66, size 4236204
[24999.871654] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
[24999.877553] omap-iommu 41501000.mmu: 41501000.mmu: version 3.0
[24999.883584] omap-iommu 41502000.mmu: 41502000.mmu: version 3.0
[24999.892308] omap-rproc 41000000.dsp: dma_alloc_coherent err: 2097152
[24999.898695] remoteproc3: Failed to process resources: -12
[24999.912976] omap_hwmod: mmu1_dsp2: _wait_target_disable failed
[24999.925941] omap_hwmod: mmu0_dsp2: _wait_target_disable failed
[24999.931827] remoteproc3: rproc_boot() failed -12
[24999.936586] virtio_rpmsg_bus: probe of virtio3 failed with error -12
[24999.942978] remoteproc3: registered virtio3 (type 7)
-----------------------------------------------
The custom resource table is slightly different between DSP1 and DSP2, because DSP2 has 8 MBytes reserved for it while DSP1 has 56 MBytes. The following resource table entries are for DSP1 and DSP2,
DSP1:
#define DSP_MEM_IPC_VRING_SIZE SZ_1M
#define DSP_MEM_IPC_DATA_SIZE SZ_1M
#define DSP_MEM_TEXT_SIZE (SZ_1M * 4)
#define DSP_MEM_DATA_SIZE (SZ_1M * 48)
#define DSP_MEM_HEAP_SIZE (SZ_1M * 3)
#define DSP_MEM_IOBUFS_SIZE (SZ_1M * 90)
DSP2:
#define DSP_MEM_IPC_VRING_SIZE SZ_1M
#define DSP_MEM_IPC_DATA_SIZE SZ_1M
#define DSP_MEM_TEXT_SIZE (SZ_1M * 1)
#define DSP_MEM_DATA_SIZE (SZ_1M * 5)
#define DSP_MEM_HEAP_SIZE (SZ_1M * 2)
#define DSP_MEM_IOBUFS_SIZE (SZ_1M * 90)
The .map files for each are as follows,
DSP1:
OUTPUT FILE NAME: <bin/release/server_dsp1.xe66>
ENTRY POINT SYMBOL: "ti_sysbios_family_c64p_Hwi0" address: 95023000
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
L2SRAM 00800000 00040000 00000000 00040000 RW X
OCMC_RAM1 40300000 00080000 00000000 00080000 RW X
OCMC_RAM2 40400000 00100000 00000000 00100000 RW X
OCMC_RAM3 40500000 00100000 00000000 00100000 RW X
EXT_CODE 95000000 00400000 0002316c 003dce94 RW X
EXT_DATA 95400000 03000000 00072ab2 02f8d54e RW
EXT_HEAP 98400000 00300000 00000000 00300000 RW
TRACE_BUF 9f000000 00060000 00008004 00057ffc RW
EXC_DATA 9f060000 00010000 00000200 0000fe00 RW
PM_DATA 9f070000 00020000 00000000 00020000 RW X
CMEM a0000000 0c000000 00000000 0c000000 RW
DSP2:
OUTPUT FILE NAME: <bin/release/server_dsp2.xe66>
ENTRY POINT SYMBOL: "ti_sysbios_family_c64p_Hwi0" address: 95023000
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
L2SRAM 00800000 00040000 00000000 00040000 RW X
OCMC_RAM1 40300000 00080000 00000000 00080000 RW X
OCMC_RAM2 40400000 00100000 00000000 00100000 RW X
OCMC_RAM3 40500000 00100000 00000000 00100000 RW X
EXT_CODE 95000000 00400000 00022f70 003dd090 RW X
EXT_DATA 95400000 03000000 00072a96 02f8d56a RW
EXT_HEAP 98400000 00300000 00000000 00300000 RW
TRACE_BUF 9f000000 00060000 00008004 00057ffc RW
EXC_DATA 9f060000 00010000 00000200 0000fe00 RW
PM_DATA 9f070000 00020000 00000000 00020000 RW X
CMEM a0000000 0c000000 00000000 0c000000 RW
As you can see EXT_CODE, EXT_DATA, and EXT_HEAP lengths match exactly between the two, which total too large for the DSP2 reserved memory.
CMEM is also being used.
In the DSP2 MainDsp2.c program the absolute path to the resource table is entered to try to avoid maybe using the wrong one, as follows,
#include "/home/user01/ti/ipc_3_44_00_00/examples/DRA7XX_linux_elf/ex02_messageq/dsp2/rsc_table_dsp.h"
and the following lines are included in DSP2.cfg to override the default resource table,
var Resource = xdc.useModule('ti.ipc.remoteproc.Resource');
Resource.customTable = true;
Does anyone know what is happening?
Thanks