Part Number: AM3352
Hi,
I think the schmatics checklist need to be corrected with respect to unused ADC.
processors.wiki.ti.com/.../AM335x_Schematic_Checklist
If ADC is not used...
Connect all TSC_ADC terminals (VREFP, VREFN, AIN[7:0], VDDA_ADC, and VSSA_ADC) to same ground as all VSS terminals.
Whereas the errata advisory says...
Advisory 1.0.32:
• TSC_ADC AIN terminals not used:
The preferred option is to have each unused AIN terminal connected to VSSA_ADC
through a 500-Ω resistor. Another option would be to leave the unused AIN terminals
open-circuit without any PCB traces connected to these terminals
Best Regards
Kummi