Other Parts Discussed in Thread: OMAP-L138, WL1271, TEST2
I am working on L138 EVM (Linux-PSP-03.20.00.12). As i need to use UART1, i enabled the UART1 in the kernel.
It' is working fine with default baud rate (115200).
Then, i tried to change the baud rate to higher values using one application (cfsetispeed + tcsetattr). It didn't work.
Table -21 of the User Guide (TMS320C674x/OMAP-L1x Processor -Universal Asynchronous Receiver/Transmitter (UART) - Literature Number: SPRUFM6B) says that maximum baud rate is 128 kbps.
Is that true?
Can i set baud rate to 3Mbps?
Thank you for your time.
Sinoj