Part Number: XTCIEVMK2LX
Hello, experts.
I'm struggling for getting data from an 3rd party ADC board with XTCIEVMK2LX (see this). Now I'm considering another approach: using an ADC EVM from TI such as ADC34J22EVM.
So, can I directly connect the ADC EVM to XTCIEVMK2LX using the FMC connector and get data in a programmatic way using RF SDK or something like that?
I know there are some showcases provided by TI which shows how to use some ADC and DAC EVMs with 66AK2L06 EVM, but the ADC EVMs are too expensive to try, and I don't need DAC attachment. So, I wonder that I can connect the ADC EVM only to the DSP-ARM EVM without the DLC card and run some test using the RF SDK tools.
Thank you very much!
ps. If this is needed to move to High Speed Data Converter forum, please do so. :)