This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4379: OpenGL ES compilation errors

Part Number: AM4379


Tool/software: Linux

Hi forum,

I am using am437xgpevm and i am trying to render a simple rectangle using sitara sdk.

#include<GLES/gl.h>
#include <GLES/glplatform.h>

void colored_rect(GLfloat left, GLfloat bottom, GLfloat right, GLfloat top, GLfloat R, GLfloat G, GLfloat B)
{
    GLfloat rect[] = {
        left, bottom,
        right, bottom,
        right, top,
        left, top
    };
    glEnableClientState(GL_VERTEX_ARRAY);
    glColor3f(R,G,B);
    glVertexPointer(2, GL_FLOAT, 0, rect);
    glDrawArrays(GL_TRIANGLE_FAN, 0, 4);
}
void main(){
	colored_rect(0,50,150,0,255,0,0);
}

I can see that the libraries are in the header files specfied but when i compile i get the following errors.

10:22:39 **** Incremental Build of configuration Debug for project gles ****
make all 
Building target: gles
Invoking: Cross GCC Linker
arm-linux-gnueabihf-gcc  -o "gles"  ./main.o   
./main.o: In function `colored_rect':
/home/alpha/workspace_v6_2/gles/Debug/../main.c:18: undefined reference to `glEnableClientState'
/home/alpha/workspace_v6_2/gles/Debug/../main.c:19: undefined reference to `glColor3f'
/home/alpha/workspace_v6_2/gles/Debug/../main.c:20: undefined reference to `glVertexPointer'
/home/alpha/workspace_v6_2/gles/Debug/../main.c:21: undefined reference to `glDrawArrays'
collect2: error: ld returned 1 exit status
make: *** [gles] Error 1

Any help would be appreciated or am i missing something here ?

Regards

-Parker