Part Number: TMS320C6670
/*
* ======== mutex.c ========
* This example shows the use of two tasks and one semaphore to perform
* mutual exclusive data access.
*/
#include<stdio.h>
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include"../INCLUDE/generate_pbch.h"
#include"../INCLUDE/phy_var.h"
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include"../INCLUDE/generate_pbch.h"
#include<string.h>
#include<stdint.h>
extern ccodelte_encode (int32_t numbits,
uint8_t add_crc,
uint8_t *inPtr,
uint8_t *outPtr,
uint16_t rnti);
extern uint32_t lte_rate_matching_cc(uint32_t RCC,
uint16_t E,
uint8_t *w,
uint8_t *e);
#define bzero(s,n) (memset((s),0,(n)))
#define LTE_NULL 2
extern uint32_t sub_block_interleaving_cc(uint32_t D, uint8_t *d,uint8_t *w);
extern int write_output(const char *fname,const char *vname,void *data,int length,int dec,char format);
extern void pbch_scrambling(LTE_DL_FRAME_PARMS *frame_parms,
uint8_t *pbch_e,
uint32_t length);
extern int allocate_pbch_REs_in_RB(LTE_DL_FRAME_PARMS *frame_parms,
int32_t **txdataF,
uint32_t *jj,
uint16_t re_offset,
uint32_t symbol_offset,
uint8_t *x0,
uint8_t pilots,
int16_t amp,
uint32_t *re_allocated);
#include <xdc/cfg/global.h>
#define AMP 128
extern unsigned int poly24a;
extern unsigned int poly8;
extern unsigned int crcbit (unsigned char * inputptr, int octetlen, unsigned int poly);
extern unsigned int crc24a (unsigned char * inptr, int bitlen);
extern unsigned int crc8 (unsigned char * inptr, int bitlen);
extern void crcTableInit ();
extern int generate_pbch(LTE_eNB_PBCH *eNB_pbch,
int32_t **txdataF,
int amp,
LTE_DL_FRAME_PARMS *frame_parms,
uint8_t *pbch_pdu,
uint8_t frame_mod4);
extern int generate_pbch(LTE_eNB_PBCH *eNB_pbch,
int32_t **txdataF,
int amp,
LTE_DL_FRAME_PARMS *frame_parms,
uint8_t *pbch_pdu,
uint8_t frame_mod4);
unsigned char pbch_pdu[6];
PHY_VARS_eNB *PHY_vars_eNB,*PHY_vars_eNB1,*PHY_vars_eNB2;
Void task1(UArg arg0, UArg arg1);
Task_Handle tsk1;
Void main()
{
Task_Params taskParams;
/* Create two tasks that share a resource*/
Task_Params_init(&taskParams);
taskParams.priority = 1;
tsk1 = Task_create (task1, &taskParams, NULL);
printf("INSIDE MAIN");
BIOS_start();
}
/*
* ======== task1 ========
*/
Void task1(UArg arg0, UArg arg1)
{
int a=10;
int b=10;
unsigned char test[] = "hey";
printf("%d\n",a+b);
printf("INSIDE TASK\n");
crcTableInit();
printf("%x\n", crcbit(test, sizeof(test) - 1, poly8));
printf("%x\n", crc8(test, (sizeof(test) - 1)*8));
printf("%x\n", crcbit(test, sizeof(test) - 1, poly24a));
printf("%x\n", crc24a(test, (sizeof(test) - 1)*8));
generate_pbch(&PHY_vars_eNB1->lte_eNB_pbch,
PHY_vars_eNB1->lte_eNB_common_vars.txdataF[0],
AMP,
&PHY_vars_eNB1->lte_frame_parms,
pbch_pdu,
0);
}
int generate_pbch(LTE_eNB_PBCH *eNB_pbch,
int32_t **txdataF,
int amp,
LTE_DL_FRAME_PARMS *frame_parms,
uint8_t *pbch_pdu,
uint8_t frame_mod4)
{
int i, l;
uint32_t pbch_D,pbch_E;//,pbch_coded_bytes;
uint8_t pbch_a[PBCH_A>>3];
uint8_t RCC;
uint32_t nsymb = (frame_parms->Ncp==NORMAL) ? 14:12;
uint32_t pilots;
#ifdef INTERFERENCE_MITIGATION
uint32_t pilots_2;
#endif
uint32_t second_pilot = (frame_parms->Ncp==NORMAL) ? 4 : 3;
uint32_t jj=0;
uint32_t re_allocated=0;
uint32_t rb, re_offset, symbol_offset;
uint16_t amask=0;
pbch_D = 16+PBCH_A;
pbch_E = (frame_parms->Ncp==NORMAL) ? 1920 : 1728; //RE/RB * #RB * bits/RB (QPSK)
// pbch_E_bytes = pbch_coded_bits>>3;
if (frame_mod4==0) {
bzero(pbch_a,PBCH_A>>3);
bzero(eNB_pbch->pbch_e,pbch_E);
memset(eNB_pbch->pbch_d,LTE_NULL,96);
// Encode data
// CRC attachment
// crc = (uint16_t) (crc16(pbch_pdu, pbch_crc_bits-16) >> 16);
/*
// scramble crc with PBCH CRC mask (Table 5.3.1.1-1 of 3GPP 36.212-860)
switch (frame_parms->nb_antennas_tx_eNB) {
case 1:
crc = crc ^ (uint16_t) 0;
break;
case 2:
crc = crc ^ (uint16_t) 0xFFFF;
break;
case 4:
crc = crc ^ (uint16_t) 0xAAAA;
break;
default:
msg("[PBCH] Unknown number of TX antennas!\n");
break;
}
*/
// Fix byte endian of PBCH (bit 23 goes in first)
for (i=0; i<(PBCH_A>>3); i++)
pbch_a[(PBCH_A>>3)-i-1] = pbch_pdu[i];
// pbch_data[i] = ((char*) &crc)[0];
// pbch_data[i+1] = ((char*) &crc)[1];
#ifdef DEBUG_PBCH
for (i=0; i<(PBCH_A>>3); i++)
msg("[PBCH] pbch_data[%d] = %x\n",i,pbch_a[i]);
#endif
if (frame_parms->mode1_flag == 1)
amask = 0x0000;
else {
switch (frame_parms->nb_antennas_tx_eNB) {
case 1:
amask = 0x0000;
break;
case 2:
amask = 0xffff;
break;
case 4:
amask = 0x5555;
}
}
ccodelte_encode(PBCH_A,2,pbch_a,eNB_pbch->pbch_d+96,amask);
#ifdef DEBUG_PBCH_ENCODING
for (i=0; i<16+PBCH_A; i++)
msg("%d : (%d,%d,%d)\n",i,*(eNB_pbch->pbch_d+96+(3*i)),*(eNB_pbch->pbch_d+97+(3*i)),*(eNB_pbch->pbch_d+98+(3*i)));
#endif //DEBUG_PBCH_ENCODING
// Bit collection
/*
j2=0;
for (j=0;j<pbch_crc_bits*3+12;j++) {
if ((pbch_coded_data[j]&0x80) > 0) { // bit is to be transmitted
pbch_coded_data2[j2++] = pbch_coded_data[j]&1;
//Bit is repeated
if ((pbch_coded_data[j]&0x40)>0)
pbch_coded_data2[j2++] = pbch_coded_data[j]&1;
}
}
#ifdef DEBUG_PBCH
msg("[PBCH] rate matched bits=%d, pbch_coded_bits=%d, pbch_crc_bits=%d\n",j2,pbch_coded_bits,pbch_crc_bits);
#endif
#ifdef DEBUG_PBCH
#ifdef USER_MODE
write_output("pbch_encoded_output2.m","pbch_encoded_out2",
pbch_coded_data2,
pbch_coded_bits,
1,
4);
#endif //USER_MODE
#endif //DEBUG_PBCH
*/
#ifdef DEBUG_PBCH_ENCODING
msg("Doing PBCH interleaving for %d coded bits, e %p\n",pbch_D,eNB_pbch->pbch_e);
#endif
RCC = sub_block_interleaving_cc(pbch_D,eNB_pbch->pbch_d+96,eNB_pbch->pbch_w);
lte_rate_matching_cc(RCC,pbch_E,eNB_pbch->pbch_w,eNB_pbch->pbch_e);
#ifdef DEBUG_PBCH_ENCODING
msg("PBCH_e:\n");
for (i=0; i<pbch_E; i++)
msg("%d %d\n",i,*(eNB_pbch->pbch_e+i));
msg("\n");
#endif
#ifdef DEBUG_PBCH
#ifdef USER_MODE
if (frame_mod4==0) {
write_output("pbch_e.m","pbch_e",
eNB_pbch->pbch_e,
pbch_E,
1,
4);
for (i=0; i<16; i++)
printf("e[%d] %d\n",i,eNB_pbch->pbch_e[i]);
}
#endif //USER_MODE
#endif //DEBUG_PBCH
// scrambling
pbch_scrambling(frame_parms,
eNB_pbch->pbch_e,
pbch_E);
#ifdef DEBUG_PBCH
#ifdef USER_MODE
if (frame_mod4==0) {
write_output("pbch_e_s.m","pbch_e_s",
eNB_pbch->pbch_e,
pbch_E,
1,
4);
for (i=0; i<16; i++)
printf("e_s[%d] %d\n",i,eNB_pbch->pbch_e[i]);
}
#endif //USER_MODE
#endif //DEBUG_PBCH
} // frame_mod4==0
// modulation and mapping (slot 1, symbols 0..3)
for (l=(nsymb>>1); l<(nsymb>>1)+4; l++) {
pilots=0;
#ifdef INTERFERENCE_MITIGATION
pilots_2 = 0;
#endif
if ((l==0) || (l==(nsymb>>1))) {
pilots=1;
#ifdef INTERFERENCE_MITIGATION
pilots_2=1;
#endif
}
if ((l==1) || (l==(nsymb>>1)+1)) {
pilots=1;
}
if ((l==second_pilot)||(l==(second_pilot+(nsymb>>1)))) {
pilots=1;
}
#ifdef DEBUG_PBCH
msg("[PBCH] l=%d, pilots=%d\n",l,pilots);
#endif
re_offset = frame_parms->ofdm_symbol_size-3*12;
symbol_offset = frame_parms->ofdm_symbol_size*l;
for (rb=0; rb<6; rb++) {
#ifdef DEBUG_PBCH
msg("RB %d, jj %d, re_offset %d, symbol_offset %d, pilots %d, nushift %d\n",rb,jj,re_offset, symbol_offset, pilots,frame_parms->nushift);
#endif
allocate_pbch_REs_in_RB(frame_parms,
txdataF,
&jj,
re_offset,
symbol_offset,
&eNB_pbch->pbch_e[frame_mod4*(pbch_E>>2)],
pilots,
#ifdef INTERFERENCE_MITIGATION
(pilots_2==1)?(amp/3):amp,
#else
amp,
#endif
&re_allocated);
re_offset+=12; // go to next RB
// check if we crossed the symbol boundary and skip DC
if (re_offset >= frame_parms->ofdm_symbol_size)
re_offset=1;
}
// }
}
#ifdef DEBUG_PBCH
printf("[PBCH] txdataF=\n");
for (i=0; i<frame_parms->ofdm_symbol_size; i++) {
printf("%d=>(%d,%d)",i,((short*)&txdataF[0][frame_parms->ofdm_symbol_size*(nsymb>>1)+i])[0],
((short*)&txdataF[0][frame_parms->ofdm_symbol_size*(nsymb>>1)+i])[1]);
if (frame_parms->mode1_flag==0) {
printf("(%d,%d)\n",((short*)&txdataF[1][frame_parms->ofdm_symbol_size*(nsymb>>1)+i])[0],
((short*)&txdataF[1][frame_parms->ofdm_symbol_size*(nsymb>>1)+i])[1]);
} else {
printf("\n");
}
}
#endif
return(0);
}
/*
* scrambling.c
*
* Created on: May 10, 2017
* Author: asmaitha
*/
#include<stdint.h>
#include"../INCLUDE/generate_pbch.h"
unsigned int lte_gold_generic(unsigned int *x1, unsigned int *x2, unsigned char reset)
{
int n;
if (reset) {
*x1 = 1+ (1<<31);
*x2=*x2 ^ ((*x2 ^ (*x2>>1) ^ (*x2>>2) ^ (*x2>>3))<<31);
// skip first 50 double words (1600 bits)
// printf("n=0 : x1 %x, x2 %x\n",x1,x2);
for (n=1; n<50; n++) {
*x1 = (*x1>>1) ^ (*x1>>4);
*x1 = *x1 ^ (*x1<<31) ^ (*x1<<28);
*x2 = (*x2>>1) ^ (*x2>>2) ^ (*x2>>3) ^ (*x2>>4);
*x2 = *x2 ^ (*x2<<31) ^ (*x2<<30) ^ (*x2<<29) ^ (*x2<<28);
}
}
*x1 = (*x1>>1) ^ (*x1>>4);
*x1 = *x1 ^ (*x1<<31) ^ (*x1<<28);
*x2 = (*x2>>1) ^ (*x2>>2) ^ (*x2>>3) ^ (*x2>>4);
*x2 = *x2 ^ (*x2<<31) ^ (*x2<<30) ^ (*x2<<29) ^ (*x2<<28);
return(*x1^*x2);
// printf("n=%d : c %x\n",n,x1^x2);
}
void pbch_scrambling(LTE_DL_FRAME_PARMS *frame_parms,
uint8_t *pbch_e,
uint32_t length)
{
int i;
uint8_t reset;
uint32_t x1, x2, s=0;
reset = 1;
// x1 is set in lte_gold_generic
x2 = frame_parms->Nid_cell; //this is c_init in 36.211 Sec 6.6.1
// msg("pbch_scrambling: Nid_cell = %d\n",x2);
for (i=0; i<length; i++) {
if ((i&0x1f)==0) {
s = lte_gold_generic(&x1, &x2, reset);
// printf("lte_gold[%d]=%x\n",i,s);
reset = 0;
}
pbch_e[i] = (pbch_e[i]&1) ^ ((s>>(i&0x1f))&1);
}
}
/*
* rate_matching.c
*
* Created on: May 10, 2017
* Author: asmaitha
*/
#include<stdint.h>
#define LTE_NULL 2
uint32_t lte_rate_matching_cc(uint32_t RCC,
uint16_t E,
uint8_t *w,
uint8_t *e)
{
uint32_t ind=0,k;
uint16_t Kw = 3*(RCC<<5);
#ifdef RM_DEBUG_CC
uint32_t nulled=0;
printf("lte_rate_matching_cc: Kw %d, E %d\n",Kw, E);
#endif
for (k=0; k<E; k++) {
while(w[ind] == LTE_NULL) {
#ifdef RM_DEBUG_CC
nulled++;
printf("RM_TX_CC : ind %d, NULL\n",ind);
#endif
ind++;
if (ind==Kw)
ind=0;
}
e[k] = w[ind];
#ifdef RM_DEBUG_CC
// printf("k %d ind %d, w %c(%d)\n",k,ind,w[ind],w[ind]);
printf("RM_TX_CC %d Ind: %d (%d)\n",k,ind,e[k]);
#endif
ind++;
if (ind==Kw)
ind=0;
}
#ifdef RM_DEBUG_CC
printf("nulled %d\n",nulled);
#endif
return(E);
}
/*
* pbch_res_allocate.c
*
* Created on: May 10, 2017
* Author: asmaitha
*/
#include<stdint.h>
#include"../INCLUDE/generate_pbch.h"
#include"../INCLUDE/phy_var.h"
#define ONE_OVER_SQRT2_Q15 23170
uint8_t is_not_pilot(uint8_t pilots, uint8_t re, uint8_t nushift, uint8_t use2ndpilots);
int allocate_pbch_REs_in_RB(LTE_DL_FRAME_PARMS *frame_parms,
int32_t **txdataF,
uint32_t *jj,
uint16_t re_offset,
uint32_t symbol_offset,
uint8_t *x0,
uint8_t pilots,
int16_t amp,
uint32_t *re_allocated)
{
MIMO_mode_t mimo_mode = (frame_parms->mode1_flag==1)?SISO:ALAMOUTI;
uint32_t tti_offset,aa;
uint8_t re;
int16_t gain_lin_QPSK;
int16_t re_off=re_offset;
uint8_t first_re,last_re;
int32_t tmp_sample1,tmp_sample2;
gain_lin_QPSK = (int16_t)((amp*ONE_OVER_SQRT2_Q15)>>15);
first_re=0;
last_re=12;
for (re=first_re; re<last_re; re++) {
tti_offset = symbol_offset + re_off + re;
// check that RE is not from Cell-specific RS
if (is_not_pilot(pilots,re,frame_parms->nushift,0)==1) {
// printf("re %d (jj %d)\n",re,*jj);
if (mimo_mode == SISO) { //SISO mapping
*re_allocated = *re_allocated + 1;
// printf("%d(%d) : %d,%d => ",tti_offset,*jj,((int16_t*)&txdataF[0][tti_offset])[0],((int16_t*)&txdataF[0][tti_offset])[1]);
for (aa=0; aa<frame_parms->nb_antennas_tx; aa++) {
((int16_t*)&txdataF[aa][tti_offset])[0] += (x0[*jj]==1) ? (-gain_lin_QPSK) : gain_lin_QPSK; //I //b_i
}
*jj = *jj + 1;
for (aa=0; aa<frame_parms->nb_antennas_tx; aa++) {
((int16_t*)&txdataF[aa][tti_offset])[1] += (x0[*jj]==1) ? (-gain_lin_QPSK) : gain_lin_QPSK; //Q //b_{i+1}
}
*jj = *jj + 1;
} else if (mimo_mode == ALAMOUTI) {
*re_allocated = *re_allocated + 1;
((int16_t*)&tmp_sample1)[0] = (x0[*jj]==1) ? (-gain_lin_QPSK) : gain_lin_QPSK;
*jj=*jj+1;
((int16_t*)&tmp_sample1)[1] = (x0[*jj]==1) ? (-gain_lin_QPSK) : gain_lin_QPSK;
*jj=*jj+1;
// second antenna position n -> -x1*
((int16_t*)&tmp_sample2)[0] = (x0[*jj]==1) ? (gain_lin_QPSK) : -gain_lin_QPSK;
*jj=*jj+1;
((int16_t*)&tmp_sample2)[1] = (x0[*jj]==1) ? (-gain_lin_QPSK) : gain_lin_QPSK;
*jj=*jj+1;
// normalization for 2 tx antennas
((int16_t*)&txdataF[0][tti_offset])[0] += (int16_t)((((int16_t*)&tmp_sample1)[0]*ONE_OVER_SQRT2_Q15)>>15);
((int16_t*)&txdataF[0][tti_offset])[1] += (int16_t)((((int16_t*)&tmp_sample1)[1]*ONE_OVER_SQRT2_Q15)>>15);
((int16_t*)&txdataF[1][tti_offset])[0] += (int16_t)((((int16_t*)&tmp_sample2)[0]*ONE_OVER_SQRT2_Q15)>>15);
((int16_t*)&txdataF[1][tti_offset])[1] += (int16_t)((((int16_t*)&tmp_sample2)[1]*ONE_OVER_SQRT2_Q15)>>15);
// fill in the rest of the ALAMOUTI precoding
if (is_not_pilot(pilots,re + 1,frame_parms->nushift,0)==1) {
((int16_t *)&txdataF[0][tti_offset+1])[0] += -((int16_t *)&txdataF[1][tti_offset])[0]; //x1
((int16_t *)&txdataF[0][tti_offset+1])[1] += ((int16_t *)&txdataF[1][tti_offset])[1];
((int16_t *)&txdataF[1][tti_offset+1])[0] += ((int16_t *)&txdataF[0][tti_offset])[0]; //x0*
((int16_t *)&txdataF[1][tti_offset+1])[1] += -((int16_t *)&txdataF[0][tti_offset])[1];
} else {
((int16_t *)&txdataF[0][tti_offset+2])[0] += -((int16_t *)&txdataF[1][tti_offset])[0]; //x1
((int16_t *)&txdataF[0][tti_offset+2])[1] += ((int16_t *)&txdataF[1][tti_offset])[1];
((int16_t *)&txdataF[1][tti_offset+2])[0] += ((int16_t *)&txdataF[0][tti_offset])[0]; //x0*
((int16_t *)&txdataF[1][tti_offset+2])[1] += -((int16_t *)&txdataF[0][tti_offset])[1];
}
re++; // adjacent carriers are taken care of by precoding
*re_allocated = *re_allocated + 1;
if (is_not_pilot(pilots,re,frame_parms->nushift,0)==0) { // skip pilots
re++;
*re_allocated = *re_allocated + 1;
}
}
}
}
return(0);
}
uint8_t is_not_pilot(uint8_t pilots, uint8_t re, uint8_t nushift, uint8_t use2ndpilots)
{
uint8_t offset = (pilots==2)?3:0;
int nushiftmod3 = nushift%3;
if (pilots==0)
return(1);
if (use2ndpilots==1) { // This is for SISO (mode 1)
if ((re!=nushift+offset) && (re!=((nushift+6+offset)%12)))
return(1);
} else { // 2 antenna pilots
if ((re!=nushiftmod3) && (re!=nushiftmod3+6) && (re!=nushiftmod3+3) && (re!=nushiftmod3+9))
return(1);
}
return(0);
}
/*
* interleaving.c
*
* Created on: May 10, 2017
* Author: asmaitha
*/
#include<stdint.h>
//static uint32_t bitrev[32] = {0,16,8,24,4,20,12,28,2,18,10,26,6,22,14,30,1,17,9,25,5,21,13,29,3,19,11,27,7,23,15,31};
//static uint32_t bitrev_x3[32] = {0,48,24,72,12,60,36,84,6,54,30,78,18,66,42,90,3,51,27,75,15,63,39,87,9,57,33,81,21,69,45,93};
static uint32_t bitrev_cc[32] = {1,17,9,25,5,21,13,29,3,19,11,27,7,23,15,31,0,16,8,24,4,20,12,28,2,18,10,26,6,22,14,30};
uint32_t sub_block_interleaving_cc(uint32_t D, uint8_t *d,uint8_t *w)
{
uint32_t RCC = (D>>5), ND, ND3;
uint32_t row,col,Kpi,index;
uint32_t index3,k;
#ifdef RM_DEBUG_CC
uint32_t nulled=0;
#endif
if ((D&0x1f) > 0)
RCC++;
Kpi = (RCC<<5);
// Kpi3 = Kpi*3;
ND = Kpi - D;
#ifdef RM_DEBUG_CC
printf("sub_block_interleaving_cc : D = %d (%d), d %p, w %p\n",D,D*3,d,w);
printf("RCC = %d, Kpi=%d, ND=%d\n",RCC,Kpi,ND);
#endif
ND3 = ND*3;
k=0;
for (col=0; col<32; col++) {
#ifdef RM_DEBUG_CC
printf("Col %d\n",col);
#endif
index = bitrev_cc[col];
index3 = 3*index;
for (row=0; row<RCC; row++) {
w[k] = d[(int32_t)index3-(int32_t)ND3];
w[Kpi+k] = d[(int32_t)index3-(int32_t)ND3+1];
w[(Kpi<<1)+k] = d[(int32_t)index3-(int32_t)ND3+2];
#ifdef RM_DEBUG_CC
printf("row %d, index %d k %d w(%d,%d,%d)\n",row,index,k,w[k],w[Kpi+k],w[(Kpi<<1)+k]);
if (w[k]== LTE_NULL)
nulled++;
if (w[Kpi+k] ==LTE_NULL)
nulled++;
if (w[(Kpi<<1)+k] ==LTE_NULL)
nulled++;
#endif
index3+=96;
index+=32;
k++;
}
}
#ifdef RM_DEBUG_CC
printf("RM_TX: Nulled %d\n",nulled);
#endif
return(RCC);
}
/* * generate_pbch.c * * Created on: May 10, 2017 * Author: asmaitha */ #include<stdio.h>
/*
* file_output.c
*
* Created on: May 10, 2017
* Author: asmaitha
*/
/*******************************************************************************
OpenAirInterface
Copyright(c) 1999 - 2014 Eurecom
OpenAirInterface is free software: you can redistribute it and/or modify
it under the terms of the GNU General Public License as published by
the Free Software Foundation, either version 3 of the License, or
(at your option) any later version.
OpenAirInterface is distributed in the hope that it will be useful,
but WITHOUT ANY WARRANTY; without even the implied warranty of
MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
GNU General Public License for more details.
You should have received a copy of the GNU General Public License
along with OpenAirInterface.The full GNU General Public License is
included in this distribution in the file called "COPYING". If not,
see <http://www.gnu.org/licenses/>.
Contact Information
OpenAirInterface Admin: openair_admin@eurecom.fr
OpenAirInterface Tech : openair_tech@eurecom.fr
OpenAirInterface Dev : openair4g-devel@lists.eurecom.fr
Address : Eurecom, Campus SophiaTech, 450 Route des Chappes, CS 50193 - 06904 Biot Sophia Antipolis cedex, FRANCE
*******************************************************************************/
//#ifdef USER_MODE
#include <string.h>
#include <stdio.h>
#include <stdlib.h>
int write_output(const char *fname,const char *vname,void *data,int length,int dec,char format)
{
FILE *fp=NULL;
int i;
printf("Writing %d elements of type %d to %s\n",length,format,fname);
if (format == 10 || format ==11 || format == 12 ) {
fp = fopen(fname,"a+");
} else if (format != 10 && format !=11 && format != 12 ) {
fp = fopen(fname,"w+");
}
if (fp== NULL) {
printf("[OPENAIR][FILE OUTPUT] Cannot open file %s\n",fname);
return(-1);
}
if (format != 10 && format !=11 && format != 12 )
fprintf(fp,"%s = [",vname);
switch (format) {
case 0: // real 16-bit
for (i=0; i<length; i+=dec) {
fprintf(fp,"%d\n",((short *)data)[i]);
}
break;
case 1: // complex 16-bit
for (i=0; i<length<<1; i+=(2*dec)) {
fprintf(fp,"%d + j*(%d)\n",((short *)data)[i],((short *)data)[i+1]);
}
break;
case 2: // real 32-bit
for (i=0; i<length; i+=dec) {
fprintf(fp,"%d\n",((int *)data)[i]);
}
break;
case 3: // complex 32-bit
for (i=0; i<length<<1; i+=(2*dec)) {
fprintf(fp,"%d + j*(%d)\n",((int *)data)[i],((int *)data)[i+1]);
}
break;
case 4: // real 8-bit
for (i=0; i<length; i+=dec) {
fprintf(fp,"%d\n",((char *)data)[i]);
}
break;
case 5: // complex 8-bit
for (i=0; i<length<<1; i+=(2*dec)) {
fprintf(fp,"%d + j*(%d)\n",((char *)data)[i],((char *)data)[i+1]);
}
break;
case 6: // real 64-bit
for (i=0; i<length; i+=dec) {
fprintf(fp,"%lld\n",((long long*)data)[i]);
}
break;
case 7: // real double
for (i=0; i<length; i+=dec) {
fprintf(fp,"%g\n",((double *)data)[i]);
}
break;
case 8: // complex double
for (i=0; i<length<<1; i+=2*dec) {
fprintf(fp,"%g + j*(%g)\n",((double *)data)[i], ((double *)data)[i+1]);
}
break;
case 9: // real unsigned 8-bit
for (i=0; i<length; i+=dec) {
fprintf(fp,"%d\n",((unsigned char *)data)[i]);
}
break;
case 10 : // case eren 16 bit complex :
for (i=0; i<length<<1; i+=(2*dec)) {
if((i < 2*(length-1)) && (i > 0))
fprintf(fp,"%d + j*(%d),",((short *)data)[i],((short *)data)[i+1]);
else if (i == 2*(length-1))
fprintf(fp,"%d + j*(%d);",((short *)data)[i],((short *)data)[i+1]);
else if (i == 0)
fprintf(fp,"\n%d + j*(%d),",((short *)data)[i],((short *)data)[i+1]);
}
break;
case 11 : //case eren 16 bit real for channel magnitudes:
for (i=0; i<length; i+=dec) {
if((i <(length-1))&& (i > 0))
fprintf(fp,"%d,",((short *)data)[i]);
else if (i == (length-1))
fprintf(fp,"%d;",((short *)data)[i]);
else if (i == 0)
fprintf(fp,"\n%d,",((short *)data)[i]);
}
printf("\n erennnnnnnnnnnnnnn: length :%d",length);
break;
case 12 : // case eren for log2_maxh real unsigned 8 bit
fprintf(fp,"%d \n",((unsigned char *)&data)[0]);
break;
}
if (format != 10 && format !=11 && format !=12 ) {
fprintf(fp,"];\n");
fclose(fp);
return(0);
} else if (format == 10 || format ==11 || format == 12 ) {
fclose(fp);
return(0);
}
return 0;
}
//#endif // USER_MODE
/*
* crc_byte.c
*
* Created on: May 10, 2017
* Author: asmaitha
*/
#include"../INCLUDE/poly.h"
unsigned int
crcbit (unsigned char * inputptr, int octetlen, unsigned int poly)
{
unsigned int i, crc = 0, c;
while (octetlen-- > 0) {
c = (*inputptr++) << 24;
for (i = 8; i != 0; i--) {
if ((1 << 31) & (c ^ crc))
crc = (crc << 1) ^ poly;
else
crc <<= 1;
c <<= 1;
}
}
return crc;
}
/*********************************************************
crc table initialization
*********************************************************/
static unsigned int crc24aTable[256];
static unsigned int crc24bTable[256];
static unsigned short crc16Table[256];
static unsigned short crc12Table[256];
static unsigned char crc8Table[256];
void crcTableInit ()
{
unsigned char c = 0;
do {
crc24aTable[c] = crcbit (&c, 1, poly24a);
crc24bTable[c] = crcbit (&c, 1, poly24b);
crc16Table[c] = (unsigned short) (crcbit (&c, 1, poly16) >> 16);
crc12Table[c] = (unsigned short) (crcbit (&c, 1, poly12) >> 16);
crc8Table[c] = (unsigned char) (crcbit (&c, 1, poly8) >> 24);
} while (++c);
}
/*********************************************************
Byte by byte implementations,
assuming initial byte is 0 padded (in MSB) if necessary
*********************************************************/
unsigned int
crc24a (unsigned char * inptr, int bitlen)
{
int octetlen, resbit;
unsigned int crc = 0;
octetlen = bitlen / 8; /* Change in octets */
resbit = (bitlen % 8);
while (octetlen-- > 0) {
// printf("in %x => crc %x\n",crc,*inptr);
crc = (crc << 8) ^ crc24aTable[(*inptr++) ^ (crc >> 24)];
}
if (resbit > 0)
crc = (crc << resbit) ^ crc24aTable[((*inptr) >> (8 - resbit)) ^ (crc >> (32 - resbit))];
return crc;
}
unsigned int crc24b (unsigned char * inptr, int bitlen)
{
int octetlen, resbit;
unsigned int crc = 0;
octetlen = bitlen / 8; /* Change in octets */
resbit = (bitlen % 8);
while (octetlen-- > 0) {
crc = (crc << 8) ^ crc24bTable[(*inptr++) ^ (crc >> 24)];
}
if (resbit > 0)
crc = (crc << resbit) ^ crc24bTable[((*inptr) >> (8 - resbit)) ^ (crc >> (32 - resbit))];
return crc;
}
unsigned int
crc16 (unsigned char * inptr, int bitlen)
{
int octetlen, resbit;
unsigned int crc = 0;
octetlen = bitlen / 8; /* Change in octets */
resbit = (bitlen % 8);
while (octetlen-- > 0) {
crc = (crc << 8) ^ (crc16Table[(*inptr++) ^ (crc >> 24)] << 16);
}
if (resbit > 0)
crc = (crc << resbit) ^ (crc16Table[((*inptr) >> (8 - resbit)) ^ (crc >> (32 - resbit))] << 16);
return crc;
}
unsigned int
crc12 (unsigned char * inptr, int bitlen)
{
int octetlen, resbit;
unsigned int crc = 0;
octetlen = bitlen / 8; /* Change in octets */
resbit = (bitlen % 8);
while (octetlen-- > 0) {
crc = (crc << 8) ^ (crc12Table[(*inptr++) ^ (crc >> 24)] << 16);
}
if (resbit > 0)
crc = (crc << resbit) ^ (crc12Table[((*inptr) >> (8 - resbit)) ^ (crc >> (32 - resbit))] << 16);
return crc;
}
unsigned int
crc8 (unsigned char * inptr, int bitlen)
{
int octetlen, resbit;
unsigned int crc = 0;
octetlen = bitlen / 8; /* Change in octets */
resbit = (bitlen % 8);
while (octetlen-- > 0) {
crc = crc8Table[(*inptr++) ^ (crc >> 24)] << 24;
}
if (resbit > 0)
crc = (crc << resbit) ^ (crc8Table[((*inptr) >> (8 - resbit)) ^ (crc >> (32 - resbit))] << 24);
return crc;
}
/*
* ccode_encode.c
*
* Created on: May 10, 2017
* Author: asmaitha
*/
#include<stdio.h>
#include<stdint.h>
unsigned short glte[] = { 0133, 0171, 0165 }; // {A,B}
unsigned short glte_rev[] = { 0155, 0117, 0127 }; // {A,B}
unsigned short gdab[] = { 0133, 0171, 0145 }; // {A,B}
unsigned short gdab_rev[] = { 0155, 0117, 0123 }; // {A,B}
unsigned char ccodelte_table[128]; // for transmitter
unsigned char ccodelte_table_rev[128]; // for receiver
extern unsigned int
crc16 (unsigned char * inptr, int bitlen);
extern unsigned int
crc8 (unsigned char * inptr, int bitlen);
void
ccodelte_encode (int32_t numbits,
uint8_t add_crc,
uint8_t *inPtr,
uint8_t *outPtr,
uint16_t rnti)
{
uint32_t state;
uint8_t c, out, first_bit;
int8_t shiftbit=0;
uint16_t c16;
uint16_t next_last_byte=0;
uint32_t crc=0;
#ifdef DEBUG_CCODE
uint32_t dummy=0;
#endif //DEBUG_CCODE
/* The input bit is shifted in position 8 of the state.
Shiftbit will take values between 1 and 8 */
state = 0;
if (add_crc == 1) {
crc = crc8(inPtr,numbits);
first_bit = 2;
c = (uint8_t)(crc>>24);
} else if (add_crc == 2) {
crc = crc16(inPtr,numbits);
#ifdef DEBUG_CCODE
printf("ccode_lte : crc %x\n",crc);
#endif
// scramble with RNTI
crc ^= (((uint32_t)rnti)<<16);
#ifdef DEBUG_CCODE
printf("ccode_lte : crc %x (rnti %x)\n",crc,rnti);
#endif
first_bit = 2;
c = (uint8_t)((crc>>16)&0xff);
} else {
next_last_byte = numbits>>3;
first_bit = (numbits-6)&7;
c = inPtr[next_last_byte-1];
}
#ifdef DEBUG_CCODE
printf("next_last_byte %x (numbits %d, %d)\n",c,numbits,next_last_byte);
#endif
// Perform Tail-biting
// get bits from last byte of input (or crc)
// for (shiftbit = first_bit; shiftbit<8; shiftbit++) {
for (shiftbit = 0 ; shiftbit <(8-first_bit) ; shiftbit++) {
if ((c&(1<<(7-first_bit-shiftbit))) != 0)
state |= (1<<shiftbit);
#ifdef DEBUG_CCODE
printf("shiftbit %d, %d -> %d \n",shiftbit,c&(1<<(7-first_bit-shiftbit)),state);
dummy+=3;
#endif
}
// get bits from next to last byte of input (not when crc is added)
if ((add_crc==0)&&((numbits&7)>0)) {
c = inPtr[next_last_byte];
// printf("last_byte %x\n",c);
// for (shiftbit = 0 ; shiftbit < (numbits&7) ; shiftbit++) {
for (shiftbit = (numbits&7)-1 ; shiftbit>=0 ; shiftbit--) {
state >>= 1;
if ((c&(1<<shiftbit)) != 0)
state |= 64;
#ifdef DEBUG_CCODE
printf("shiftbit %d, %d: %d -> %d \n",shiftbit,state>>6,dummy,state);
dummy+=3;
#endif
}
}
state = state & 0x3f; // true initial state of Tail-biting CCode
state<<=1; // because of loop structure in CCode
#ifdef DEBUG_CCODE
printf("Initial state %d\n",state);
dummy = 0;
#endif //DEBUG_CCODE
/* Do not increment inPtr until we read the next octet */
while (numbits > 0) {
c = *inPtr++;
#ifdef DEBUG_CCODE
printf("** %x **\n",c);
#endif //DEBUG_CCODE
// for (shiftbit = 0; (shiftbit<8) && (numbits>0);shiftbit++,numbits--) {
for (shiftbit = 7; (shiftbit>=0) && (numbits>0); shiftbit--,numbits--) {
state >>= 1;
if ((c&(1<<shiftbit)) != 0) {
state |= 64;
}
out = ccodelte_table[state];
*outPtr++ = out & 1;
*outPtr++ = (out>>1)&1;
*outPtr++ = (out>>2)&1;
#ifdef DEBUG_CCODE
printf("numbits %d, input %d, outbit %d: %d -> %d (%d%d%d)\n",numbits,state>>6,dummy,state,out,out&1,(out>>1)&1,(out>>2)&1);
dummy+=3;
#endif //DEBUG_CCODE
}
}
// now code 8-bit CRC for UCI
if (add_crc == 1) {
c = (uint8_t)(crc>>24);
// for (shiftbit = 0; (shiftbit<8);shiftbit++) {
for (shiftbit = 7; (shiftbit>=0); shiftbit--) {
state >>= 1;
if ((c&(1<<shiftbit)) != 0) {
state |= 64;
}
out = ccodelte_table[state];
*outPtr++ = out & 1;
*outPtr++ = (out>>1)&1;
*outPtr++ = (out>>2)&1;
#ifdef DEBUG_CCODE
printf("crc bit %d input %d, outbit %d: %d -> %d (%d)\n",shiftbit,state>>6,dummy,state,out,ccodelte_table[state]);
dummy+=3;
#endif //DEBUG_CCODE
}
}
// now code 16-bit CRC for DCI
if (add_crc == 2) {
c16 = (uint16_t)(crc>>16);
// for (shiftbit = 0; (shiftbit<16);shiftbit++) {
for (shiftbit = 15; (shiftbit>=0); shiftbit--) {
state >>= 1;
if ((c16&(1<<shiftbit)) != 0) {
state |= 64;
}
out = ccodelte_table[state];
*outPtr++ = out & 1;
*outPtr++ = (out>>1)&1;
*outPtr++ = (out>>2)&1;
#ifdef DEBUG_CCODE
printf("crc bit %d input %d, outbit %d: %d -> %d (%d)\n",shiftbit,state>>6,dummy,state,out,ccodelte_table[state]);
dummy+=3;
#endif //DEBUG_CCODE
}
}
}
I'm using CCSv5 . I'm working on PBCH . My code is compiled and debugged correctly . The problem i'm facing is in running that code. When i'm creating a task and as i'm entering to a function inside that task it gets terminated over there. I've attached all the files. Kindly go through all these files and tell me the possible answer for that.
Thanks,
Lalit