Part Number: OMAP-L138
Other Parts Discussed in Thread: OMAPL138, SYSBIOS
Tool/software: TI-RTOS
Hello,
I am using SYSBIOS 6.34.03.19 and pdk_OMAPL138 1.01.00.02. The McASP example project has a typedef in mcasp_drv.h that specifies the various buffer formats available from the driver, but there is not much information as to exactly what these formats look like. It does, however, mention a user guide that explains it more. I checked the McASP_LLD_Design.pdf document provided with the driver and found references to buffer formats, but no explanation of the definitions. Am I looking in the wrong place, or is the documentation incomplete?
It would be convenient if the EDMA PaRAM configurations provided here would accomplish the deinterleaving I need (put each received channel into a separate buffer), so I would like to check before I modify the code unnecessarily.
Jeff