Part Number: DM388
Tool/software: Linux
Dear Sir,
From the TRM, I know DM388 has 12 on-chip PLL at top level.
I want to disable the useless PLL for power saving. Ex, SATA, PCIe, Ethernet MAC.
I change the file "ti81xx-clock.tdsi" via "ti,set-bit-to-disable;"
For example, I hope to disable PLL_VIDEO0 (Is it ARM M3?) to check the current.
/* Clock input select for video0 DPLL */
video0_dpll_clkin_ck: video0_dpll_clkin_ck {
#clock-cells = <0>;
compatible = "ti,mux-clock";
clocks = <&devosc_ck>;
reg = <0x02C0>; /* OSC_SRC Register */
/*ti,bit-shift = <16>;*/
ti,set-bit-to-disable;
};
After do that, I don't get the correct action, The current doesn't change.
Can you give me a example how to do that?
Thanks.
S.K.