This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am5728: RGMII transition time specification

Guru 10235 points

Part Number: AM5728

Hello, TI Experts,

 

Our customer sent us a question from the datasheet(SPRS953B) "Table 7-81. Timing Requirements for rgmiin_rxc - RGMIIn Operation"

and "Figure 7-59. GMAC Receive Interface Timing, RGMIIn operation".

 

Question:

  Regarding the specification of "Transition time, rgmiin_rxc" MAX:0.75ns,

  Which understanding is correct for the definition of voltage changing range as below?

     1) +0.8V~+2.0V ( The spec. [ VIL=0.8V, VIH=2.0V]  is found from datasheet(SPRS953B) "Table 5-17" )

     2) 20%-80%

 

They also said "BUFFER TYPE is Dual Voltage LVCMOS(3.3V_Mode)".

 

Best regards,