This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP/BIOS 5.41.05.20

The release notes for DSP/BIOS 5.41.06.21 reference DSP/BIOS 5.41.05.20 for which I find no release notes, are the only changes between 04.18 and 06.21 those listed in the release notes or were there extras in 05.20 ?

Peter Myerscough-Jackopson

  • For some reason, 5.41.05 is not posted on external web.   It contains fixes for the following 3 issues.

    Note that we include release notes for previous products in the 'docs/relnotes_archive' folder, but that requires you to install 5.41.06 to see the 5.41.05 release notes.

    We will either post 5.41.05 externally, or at least post the release notes.  

    Here's the changes in 5.41.05 from 5.41.04.

    What's New

    • CCSv4 users will need to check their installed CCS version has XDCtools version 3.16.03 or higher to use the product for evm5515.   The XDCtools product can be downloaded here.
    • Enchanements and Defects Fixed:
    id                                Headline
    SDOCM00071149    MEM ROV view in CCS 4.x is messed up when doing MEM_define or MEM_increaseTableSize
    SDOCM00068907    Add examples back into BIOS 5.41.xx via project wizard (CCSv4.2 or higher)
    SDOCM00053554    Kernel/Object View (KOV) has problems on 28x for heaps with size > 64K