Other Parts Discussed in Thread: TVP5158
Hi, all
I doubt the following question when i configure the CCDC(DM6441) to interact with the codec chip, TW2864:
1) the output of TW2864 chip is 4 channel CIF Time-multiplexed format BT.656 with 54MHZ which is not standard BT.656 but time-multiplexed, so the CCDC is configured
as RAW mode to accept the data. in hardware, i only connect the TW2864'S PCLK and 8 output data line into CCDC's plck and CCD[7:0] respectively, and no VD/HD/C_FIELD. is there anything wrong? if that's right, what i doubt is: what's the condition of VDINT0 and VDINT1 if no external VD/HD input?
2) In my case, the RAW mode is the only choice ? or is there some other choice, such as YUV interface?
BR,
-JASON