This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms320c5517: CLKIN input ranges

Part Number: TMS320C5517
Other Parts Discussed in Thread: TMS320C5517

For Boot Mode, I see on TMS320C5517 datasheet some limits for CLKIN

00:
CLK_SEL = 0: 12 MHz via the on-chip USB oscillator
CLK_SEL = 1: 11.2896 MHz via the CLK_IN pin
01:
CLK_SEL = 0: 12 MHz via the on-chip USB oscillator
CLK_SEL = 1: 12.00 MHz or 12.288 MHz via the CLK_IN pin
10:
CLK_SEL = 0: 12 MHz via the on-chip USB oscillator
CLK_SEL = 1: 16.8 MHz via the CLK_IN pin
11:
CLK_SEL = 0: 12 MHz via the on-chip USB oscillator
CLK_SEL = 1: 19.2 MHz via the CLK_IN pin

Datasheet shows only "typical" or nominal CLK_IN values: which are min and max values for CLK_IN ? Is it possible to set a CLK_IN which is multiple of 65536 Hz ?