Tool/software: Linux
I am developing a QT based GUI application for a custom hardware based on TI EVM AM572X and the processor SDK I am using for cross compilation is ti-processor-sdk-linux-am57xx-evm-03.03.00.04-Linux-x86-Install.bin. There are multiple buttons on the GUI application. On random click of the buttons the application quits with the message "Did the WayLand compositor die ? " after intermittent time interval . When I check the display service /usr/bin/runWeston , it has stopped running.
Please kindly help me if there is a version issue of wayland as the version of Wayland being used is 1.9.0. There are no exception caught and thrown from the Qt application.
Thanks and Regards
vaishnav