Part Number: AM3357
Other Parts Discussed in Thread: AM3352, TPS65910
Tool/software: Linux
Hello Sir,
I am trying to bring up the ethernet (eth0) which is properly working in uboot but not working wen linux is booted
here is the kernel booting log
kindly go through this log,
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.19-gdb0b54cdad (root@adems) (gcc version 5.4.0 20160609 (Ubuntu/Linaro 5.4.0-6ubuntu1~16.04.4) ) #1 PREEMPT T7
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM
[ 0.000000] cma: Reserved 24 MiB at 0xbe800000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 260416
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=ubi0:rootfs rw ubi.mtd=NAND.file-system,2048 rootfstype=ubifs rootwait=1
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 1004012K/1048576K available (6571K kernel code, 313K rwdata, 2324K rodata, 260K init, 265K bss, 19988K reserved, 24576K)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08b8004 (8897 kB)
[ 0.000000] .init : 0xc08b9000 - 0xc08fa000 ( 260 kB)
[ 0.000000] .data : 0xc08fa000 - 0xc0948610 ( 314 kB)
[ 0.000000] .bss : 0xc0948610 - 0xc098ad18 ( 266 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000040] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000053] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000252] clocksource_probe: no matching clocksources found
[ 0.000467] Console: colour dummy device 80x30
[ 0.000498] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000506] This ensures that you still see kernel messages. Please
[ 0.000514] update your kernel commandline.
[ 0.000537] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.058793] pid_max: default: 32768 minimum: 301
[ 0.058964] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.058982] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.059845] Initializing cgroup subsys io
[ 0.059883] Initializing cgroup subsys memory
[ 0.059928] Initializing cgroup subsys devices
[ 0.059947] Initializing cgroup subsys freezer
[ 0.059965] Initializing cgroup subsys perf_event
[ 0.059980] Initializing cgroup subsys pids
[ 0.060014] CPU: Testing write buffer coherency: ok
[ 0.060468] Setting up static identity map for 0x80008200 - 0x80008258
[ 0.063207] devtmpfs: initialized
[ 0.078229] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.096375] omap_hwmod: debugss: _wait_target_disable failed
[ 0.153629] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.156233] pinctrl core: initialized pinctrl subsystem
[ 0.157828] NET: Registered protocol family 16
[ 0.160528] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.188852] cpuidle: using governor ladder
[ 0.218841] cpuidle: using governor menu
[ 0.224588] OMAP GPIO hardware version 0.1
[ 0.234939] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_s0, deferrie
[ 0.237575] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.279655] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.284669] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring e
[ 0.284853] media: Linux media interface: v0.10
[ 0.284942] Linux video capture interface: v2.00
[ 0.285010] pps_core: LinuxPPS API ver. 1 registered
[ 0.285021] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.285059] PTP clock support registered
[ 0.285131] EDAC MC: Ver: 3.0.0
[ 0.286535] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.286948] Advanced Linux Sound Architecture Driver Initialized.
[ 0.288411] clocksource: Switched to clocksource timer1
[ 0.302316] NET: Registered protocol family 2
[ 0.303279] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.303397] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.303506] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.303629] UDP hash table entries: 512 (order: 1, 8192 bytes)
[ 0.303666] UDP-Lite hash table entries: 512 (order: 1, 8192 bytes)
[ 0.303854] NET: Registered protocol family 1
[ 0.304333] RPC: Registered named UNIX socket transport module.
[ 0.304350] RPC: Registered udp transport module.
[ 0.304359] RPC: Registered tcp transport module.
[ 0.304367] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.305231] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.307716] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.318357] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.319745] NFS: Registering the id_resolver key type
[ 0.319828] Key type id_resolver registered
[ 0.319840] Key type id_legacy registered
[ 0.319929] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.320303] jffs2: version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
[ 0.324770] bounce: pool size: 64 pages
[ 0.325087] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 248)
[ 0.325114] io scheduler noop registered
[ 0.325130] io scheduler deadline registered
[ 0.325327] io scheduler cfq registered (default)
[ 0.326746] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.409391] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.414616] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.035075] console [ttyS0] enabled
[ 1.040092] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.050305] [drm] Initialized drm 1.1.0 20060810
[ 1.057376] tilcdc 4830e000.lcdc: no encoders/connectors found
[ 1.072536] loop: module loaded
[ 1.079120] libphy: Fixed MDIO Bus: probed
[ 1.148493] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.154640] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 1.161883] libphy: 4a101000.mdio: probed
[ 1.165934] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver TI DP83867
[ 1.175140] cpsw 4a100000.ethernet: No slave[1] phy_id, phy-handle, or fixed-link property
[ 1.183573] cpsw 4a100000.ethernet: Detected MACID = 68:c9:0b:75:13:63
[ 1.191977] mousedev: PS/2 mouse device common for all mice
[ 1.198299] i2c /dev entries driver
[ 1.203290] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.211105] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.362421] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.373303] NET: Registered protocol family 10
[ 1.379542] sit: IPv6 over IPv4 tunneling driver
[ 1.385173] NET: Registered protocol family 17
[ 1.390175] Key type dns_resolver registered
[ 1.394683] omap_voltage_late_init: Voltage driver support not added
[ 1.405093] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.410466] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.418242] nand: device found, Manufacturer ID: 0x2c, Chip ID: 0xda
[ 1.424762] nand: Micron MT29F2G08ABAEAWP
[ 1.428845] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 64
[ 1.436484] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.441960] 10 ofpart partitions found on MTD device 8000000.nand
[ 1.448086] Creating 10 MTD partitions on "8000000.nand":
[ 1.453541] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.460454] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.467844] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.475333] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.482628] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[ 1.490146] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 1.497270] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 1.504558] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 1.512539] 0x000000200000-0x000000a00000 : "NAND.kernel"
[ 1.522257] 0x000000a00000-0x000010000000 : "NAND.file-system"
[ 1.638666] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.669284] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.675724] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.681006] vmmc: supplied by vbat
[ 1.719214] vdd_mpu: supplied by vbat
[ 1.729444] ubi0: attaching mtd9
[ 3.690883] ubi0: scanning is finished
[ 3.719993] ubi0: attached mtd9 (name "NAND.file-system", size 246 MiB)
[ 3.726727] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes
[ 3.733715] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 512
[ 3.740524] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096
[ 3.747568] ubi0: good PEBs: 1968, bad PEBs: 0, corrupted PEBs: 0
[ 3.753764] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128
[ 3.761096] ubi0: max/mean erase counter: 2/0, WL threshold: 4096, image sequence number: 1634636836
[ 3.770340] ubi0: available PEBs: 0, total reserved PEBs: 1968, PEBs reserved for bad PEB handling: 40
[ 3.779768] ubi0: background thread "ubi_bgt0d" started, PID 58
[ 3.787282] hctosys: unable to open rtc device (rtc0)
[ 3.796794] lis3_reg: disabling
[ 3.800078] wlan-en-regulator: disabling
[ 3.804473] ALSA device list:
[ 3.807464] No soundcards found.
[ 3.818535] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 59
[ 3.873041] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "rootfs"
[ 3.880661] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes
[ 3.890663] UBIFS (ubi0:0): FS size: 242905088 bytes (231 MiB, 1913 LEBs), journal size 9023488 bytes (8 MiB, 72 LEBs)
[ 3.901425] UBIFS (ubi0:0): reserved for root: 0 bytes (0 KiB)
[ 3.907295] UBIFS (ubi0:0): media format: w4/r0 (latest is w4/r0), UUID 33E743D7-4D43-4A54-B4C7-7700F91F2C19, small LPT model
[ 3.920248] VFS: Mounted root (ubifs filesystem) on device 0:14.
[ 3.927824] devtmpfs: mounted
[ 3.931301] Freeing unused kernel memory: 260K (c08b9000 - c08fa000)
[ 3.937684] This architecture does not have kernel memory protection.
[ 4.146419] systemd[1]: System time before build time, advancing clock.
[ 4.213890] random: systemd: uninitialized urandom read (16 bytes read, 10 bits of entropy available)
[ 4.245831] random: systemd: uninitialized urandom read (16 bytes read, 10 bits of entropy available)
[ 4.269185] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCR)
[ 4.289042] systemd[1]: Detected architecture arm.
Welcome to Arago 2016.08!
[ 4.320747] systemd[1]: Set hostname to <am335x-evm>.
[ 4.505874] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 4.549819] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 4.612078] random: systemd: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 4.672909] random: systemd: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 4.682941] random: systemd: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 4.693573] random: systemd: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 4.761753] random: systemd: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 4.794289] random: systemd: uninitialized urandom read (16 bytes read, 11 bits of entropy available)
[ 5.074146] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 5.113798] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 5.164197] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 5.189447] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 5.218965] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 5.250405] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 5.281250] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 5.317078] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 5.354415] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 5.414267] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 5.559582] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 5.625922] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 5.676349] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ 5.724276] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 5.778931] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
[ 5.799177] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 5.829992] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 5.859180] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 5.889279] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 5.924158] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.959077] systemd[1]: Reached target Paths.
[ OK ] Reached target Paths.
[ 5.994440] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 6.050761] systemd[1]: Created slice system-getty.slice.
[ OK ] Created slice system-getty.slice.
[ 6.066572] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 6.099359] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 6.167958] systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
[ 6.209297] systemd[1]: Mounted POSIX Message Queue File System.
[ OK ] Mounted POSIX Message Queue File System.
[ 6.229214] systemd[1]: Mounted Temporary Directory.
[ OK ] Mounted Temporary Directory.
[ 6.259872] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Started Setup Virtual Console.
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
Starting Create Static Device Nodes in /dev...
Starting udev Coldplug all Devices...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Create Static Device Nodes in /dev.
[ 8.031539] systemd-journald[102]: Received request to flush runtime journal from PID 1
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Mounting /media/ram...
Starting udev Kernel Device Manager...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started udev Kernel Device Manager.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
[ 10.318380] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 10.448753] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc0
[ OK ] Found device /dev/ttyS0.
[ OK ] Started udev Coldplug all Devices.
[ 10.913666] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 11.382909] ti-pruss 4a300000.pruss: creating PRU cores and other child platform devices
[ 11.510144] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 11.517939] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 11.793998] remoteproc0: 4a334000.pru0 is available
[ 11.828636] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 11.837675] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ 12.092627] remoteproc0: Direct firmware load for am335x-pru0-fw failed with error -2
[ 12.158614] remoteproc0: failed to load am335x-pru0-fw
[ 12.163936] pru-rproc 4a334000.pru0: booting the PRU core manually
[ 12.248724] remoteproc0: powering up 4a334000.pru0
[ 12.253735] remoteproc0: Direct firmware load for am335x-pru0-fw failed with error -2
[ 12.378705] remoteproc0: request_firmware failed: -2
[ 12.383822] pru-rproc 4a334000.pru0: rproc_boot failed
[ 12.496596] remoteproc0: releasing 4a334000.pru0
[ 12.571630] pru-rproc: probe of 4a334000.pru0 failed with error -2
[ 12.688677] remoteproc0: 4a338000.pru1 is available
[ 12.693702] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 12.843933] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 12.896147] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 13.026694] remoteproc0: Direct firmware load for am335x-pru1-fw failed with error -2
[ 13.083009] remoteproc0: failed to load am335x-pru1-fw
[ 13.088343] pru-rproc 4a338000.pru1: booting the PRU core manually
[ 13.131116] remoteproc1: wkup_m3 is available
[ 13.135611] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 13.148640] remoteproc0: powering up 4a338000.pru1
[ 13.153649] remoteproc0: Direct firmware load for am335x-pru1-fw failed with error -2
[ OK ] Started Network Time Synchronization.
[ 13.279393] remoteproc0: request_firmware failed: -2
[ 13.284511] pru-rproc 4a338000.pru1: rproc_boot failed
[ 13.324317] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 13.419314] remoteproc0: releasing 4a338000.pru1
[ 13.424217] pru-rproc: probe of 4a338000.pru1 failed with error -2
[ 13.446739] wkup_m3_ipc 44e11324.wkup_m3_ipc: could not get rproc handle
[ 13.624352] remoteproc1: powering up wkup_m3
[ 13.679799] remoteproc1: Booting fw image am335x-pm-firmware.elf, size 217148
[ 13.687366] remoteproc1: remote processor wkup_m3 is now up
[ 13.693083] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x191
[ 13.862938] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 14.462724] PM: bootloader does not support rtc-only!
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Found device /dev/ttyS3.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
Starting Synchronize System and HW clocks...
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Synchronize System and HW clocks.
[ OK ] Reached target System Initialization.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
Starting Print notice about GPLv3 packages...
[ OK ] Started Kernel Logging Service.
[ OK ] Started System Logging Service.
Starting Login Service...
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
Starting telnetd.service...
Starting Permit User Sessions...
[ OK ] Started D-Bus System Message Bus.
[ 18.386042] usbcore: Unknown symbol usb_put_phy (err 0)
[ 18.434658] usbcore: Unknown symbol usb_otg_kick_fsm (err 0)
Starting Network Service...
[ OK ] Started telnetd.service.[ 18.519304] usbcore: Unknown symbol usb_speed_string (err 0)
[ 18.527910] usbcore: Unknown symbol usb_otg_unregister_hcd (err 0)
[ OK ] Started Permit User Sessions.
[ 18.678958] usbcore: Unknown symbol usb_hcd_amd_remote_wakeup_quirk (err 0)
[ 18.686006] usbcore: Unknown symbol usb_get_phy_dev (err 0)
[ 18.797310] usbcore: Unknown symbol usb_otg_register_hcd (err 0)
[ 18.849958] usbcore: Unknown symbol usb_put_phy (err 0)
[ 18.855277] usbcore: Unknown symbol usb_otg_kick_fsm (err 0)
[ 18.911753] usbcore: Unknown symbol usb_speed_string (err 0)
[ 18.917611] usbcore: Unknown symbol usb_otg_unregister_hcd (err 0)
[ 19.039058] usbcore: Unknown symbol usb_hcd_amd_remote_wakeup_quirk (err 0)
[ 19.046107] usbcore: Unknown symbol usb_get_phy_dev (err 0)
[ 19.161148] usbcore: Unknown symbol usb_otg_register_hcd (err 0)
[ 19.202563] usbcore: Unknown symbol usb_put_phy (err 0)
[ 19.207883] usbcore: Unknown symbol usb_otg_kick_fsm (err 0)
[ 19.298957] usbcore: Unknown symbol usb_speed_string (err 0)
[ 19.304813] usbcore: Unknown symbol usb_otg_unregister_hcd (err 0)
[ 19.402487] usbcore: Unknown symbol usb_hcd_amd_remote_wakeup_quirk (err 0)
[ 19.514319] usbcore: Unknown symbol usb_get_phy_dev (err 0)
[ 19.560906] usbcore: Unknown symbol usb_otg_register_hcd (err 0)
[ 19.607328] usbcore: Unknown symbol usb_put_phy (err 0)
[ 19.641383] usbcore: Unknown symbol usb_otg_kick_fsm (err 0)
[ 19.647771] usbcore: Unknown symbol usb_speed_string (err 0)
[ 19.696292] usbcore: Unknown symbol usb_otg_unregister_hcd (err 0)
[ 19.738982] usbcore: Unknown symbol usb_hcd_amd_remote_wakeup_quirk (err 0)
[ 19.746030] usbcore: Unknown symbol usb_get_phy_dev (err 0)
[ 19.798758] usbcore: Unknown symbol usb_otg_register_hcd (err 0)
[ OK ] Started Network Service.
[ 20.052561] net eth0: initializing cpsw version 1.12 (0)
[ 20.057963] net eth0: initialized cpsw ale version 1.4
[ 20.078616] net eth0: ALE Table size 1024
[ 20.084975] net eth0: phy "4a101000.mdio:00" not found on slave 0, err -19
[ 20.130436] libphy: PHY not found
[ 20.133898] net eth0: phy "" not found on slave 1, err -19
[ 20.173878] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
binutils
dosfstools
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ OK ] Started Login Service.
[ OK ] Reached target Network.
Starting Network Name Resolution...
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
Starting thttpd.service...
[ OK ] Started thttpd.service.
[ OK ] Started Network Name Resolution.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
Starting thermal-zone-init.service...
[ OK ] Started thermal-zone-init.service.
[ 28.720648] random: nonblocking pool is initialized