Hi all,
Before we get PCB's manufactured I want to ensure our schematic is correct (so that if we have any issues, we can be fairly confident that it is PCB stackup and/or physical routing related). I have subsequently removed various MUX's as well as the CPLD from the DVEVM and begun to hard wire tracks manually. This will also allow us to start modifying linux drivers in preparation for when our PCBs arrive.
Unlike the Ethernet & Video MUXs however, the CPLD however is a rather complex bugger - particularly when it comes to the power & PRTC sub systems because of its criticality (and my current lack of complete understanding). I have not powered up the board since removing the CPLD as I am concerned about the power sequencing as well as being uncertain as to why some of the IO are routed into the CPLD as they are. I have downloaded the CPLD firmware .zip from Spectrum Digital & wish to try investigate in a bit more detail what it is doing. Can anyone recommend what I can use to open these files (freeware)? I do not want to reprogram the CPLD, merely see what it is currently doing to better get our boards up and running without it.
Sincerely,
NickA