Part Number: AM5728
Other Parts Discussed in Thread: AM3358
Tool/software: Linux
Hi,
I am new to AM572x EVM. Previously I worked with Beaglebone Black and interfaced GPIOs, UART and I2C.
But I think , it is slightly different for AM572x EVM.
Please refer me some wiki or guides , for interfacing GPIOs, UARTs and I2C inAM572x.
Now I am able to communicate with AM572x EVM through ssh(Ethernet port), minicom(debug port).
And I can run some simple applications - helloworld.
First I tested GPIOs with the same code which is working well in Beaglebone black board.
With this software, the folder /sys/class/gpio/gpioxx folders are getting created. The file "value" is getting updated as in the software.
But this value is not appeared in the pin output.
Shall I change the am57xx_evm.dts file to make GPIOs, UART and I2C working for AM572x?
Thanks in advance for the help.
Thanks and Regards,
Sajeevan.K