Part Number: AM3352
Tool/software: Linux
Hi,
We have ported linux-4.4.12 based sdk and with this lcdc driver is reporting 6500 KHz clock in drm debug log which is as per dts file.
But when I probe it on CRO it reports 32MHz even I change clock to any value it is reporting as 32MHz on CRO. Which is resulting flicker and aliasing effect on lcd. LCD dimensions are 320x240.
We had same product on linux-3.2.0 based psp but it is reporting correct 6.5MHz.
What is change in new drm based driver and old fbdev driver and what we are doing wrong ?
BR,
Rohit Khatri