Part Number: AM3352
Posting on behalf of the field team
---
One of my customers designing IOT gateway based on AM335x (300 MHz) device without PMIC to save the cost. But they need the RTC feature. From the power perspective only the power sequencing needs to be done and as DVFS is not supported and we support only the DS1 , no Linux driver is required here right ?
Also they need some mechanism to wake up the system from internally like the RTC alarm. For this they can use the AM335x internal RTC right ?