Other Parts Discussed in Thread: AM3505
Where can i find the maximum output current of the AM3505/17 LVCMOS GPIOs?
Can't find it in the documentation.
thanks
fred
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Fred,
I am working to get these values added in the data sheet, but until then, here are the values you are looking for.
IOH = -2mA
IOL = 2mA
Input current for dual voltage IO pins:
II (without internal resistor) = +/-9uA
II (With internal pullup) = min 70uA; max 310uA
II (with internal pull down) = min -75uA; max -270uA
Input current for DDR2/mDDR 1.8v IO pins:
II (with internal pull down resistor) = min -77uA; max -286uA
IOZ (without pull) = +/-20uA
Best regards,
Jeff
Hello Fred,
The +/-2mA does have margin. Those numbers are the same as used on the OMAP35x devices.
For the latchup current, testing follows the jedec spec. 100C, +/-100mA, 1.5xVdd level. Is that what you are looking for?
Thanks,
Jeff