This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMDSICE3359: DP83630 Linux driver

Part Number: TMDSICE3359

Tool/software: Linux

Hello,

I have some questions about the Ethernet transceiver of DP83630:

we have used the demo board TMDSICE3359 with the ethernet transceiver of TLK1100. We have made the image of LinuxRT with SDK. We have made own board with ethernet transceiver of DP83630. LinuxRT worked at the TMDSICE3359, and this linuxRT is launched at the own board, but ethernet interfaces has not worked. DO you have the recommendations / files how I can include the driver  ethernet transceiver of DP8360 to LinuxRT. Does The firmware support the units of PRU, which has included in the actual version SDK?

 


When will SDK for LinuxRT (Processor-SDK-linux-RT-AM335X) version 3.3 available for AM335X. Or how can I adapt the solution of AM572x for AM335X (demo board TMDSICE3359)