This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM6467:Can't boot Linux .



after I burn myself build image to the DAVINCI,it run as follows:

 

DM6467 EVM > boot

NAND read: device 0 offset 0x560000, size 0x500000
 5242880 bytes read: OK

Loading from NAND 128MiB 3,3V 8-bit, offset 0x160000
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1971144 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1971144 Bytes =  1.9 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
...................................................................... done, boo
ting the kernel.

===========================

It stoped here for ever. I don't know WHY?