Our company just got a new batch of prototypes and are having some trouble with HPI booting the new boards. The DSP will boot via JTAG with CCS IDE, but not through the host. There are very few differences between the boards but one difference is the DSP silicon revision. The current boards are rev A (1.1) device and the new boards are rev B (2.0) device. Is there any known issues (or deltas) with this new rev. that would explain this problem?
The PCBs are the same. The host processor is the same. Only minor component changes. When the HPI boot is attempted, the load completes and the code starts executing but halts (or crashes) soon after. An LED will start to blink and some text will start to come out the UART but then it stops. This same image can be HPI boot loaded on the original batch of boards we had made.
thanks in advance,
Mike