Part Number: AM3358
Tool/software: Linux
Hello,
I'm interfacing the chipsee LCD with new SDK version 03.03.00.04 from TI. I'm able to bring up LCD basically, stuck with completely with touch screen
I have the following issues:
1. Touch screen is not working, not able to calibrate. But as per kernel log driver probing.
U-Boot SPL 2016.05-g4db46a6bbd (Mar 29 2017 - 17:44:45)
Trying to boot from MMC1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-g4db46a6bbd (Mar 29 2017 - 17:44:45 -0400)
CPU : AM335X-GP rev 2.1
Model: TI AM335x BeagleBone Black
Watchdog enabled
DRAM: 512 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in SROM is de:ad:be:ef:00:01
Address in environment is 04:a3:16:f8:0e:5e
, eth1: usb_ether
Press SPACE to abort autoboot in 2 seconds
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3493920 bytes read in 1207 ms (2.8 MiB/s)
39317 bytes read in 38 ms (1009.8 KiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x355020 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff3000, end 8ffff994 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.41-gf9f6f0db2d (root@fg-1) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #11 PREEMPT Wed May 17 19:02:29 IST 2017
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x BeagleBone Black
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=000c50d8-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 459912K/524288K available (6627K kernel code, 325K rwdata, 2384K rodata, 272K init, 265K bss, 15224K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08d5004 (9013 kB)
[ 0.000000] .init : 0xc08d6000 - 0xc091a000 ( 272 kB)
[ 0.000000] .data : 0xc091a000 - 0xc096b630 ( 326 kB)
[ 0.000000] .bss : 0xc096b630 - 0xc09add58 ( 266 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000015] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000033] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000041] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000190] clocksource_probe: no matching clocksources found
[ 0.000343] Console: colour dummy device 80x30
[ 0.000367] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000373] This ensures that you still see kernel messages. Please
[ 0.000377] update your kernel commandline.
[ 0.000394] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089238] pid_max: default: 32768 minimum: 301
[ 0.089353] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089363] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089969] Initializing cgroup subsys io
[ 0.089997] Initializing cgroup subsys memory
[ 0.090031] Initializing cgroup subsys devices
[ 0.090044] Initializing cgroup subsys freezer
[ 0.090056] Initializing cgroup subsys perf_event
[ 0.090066] Initializing cgroup subsys pids
[ 0.090089] CPU: Testing write buffer coherency: ok
[ 0.090449] Setting up static identity map for 0x80008200 - 0x80008260
[ 0.092248] devtmpfs: initialized
[ 0.102660] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.115464] omap_hwmod: debugss: _wait_target_disable failed
[ 0.170904] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.174415] pinctrl core: initialized pinctrl subsystem
[ 0.175597] NET: Registered protocol family 16
[ 0.177417] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.199230] cpuidle: using governor ladder
[ 0.229221] cpuidle: using governor menu
[ 0.233014] OMAP GPIO hardware version 0.1
[ 0.242158] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.276277] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.279604] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.279658] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.279689] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe
[ 0.279803] media: Linux media interface: v0.10
[ 0.279855] Linux video capture interface: v2.00
[ 0.279897] pps_core: LinuxPPS API ver. 1 registered
[ 0.279903] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.279948] PTP clock support registered
[ 0.279995] EDAC MC: Ver: 3.0.0
[ 0.281012] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.281319] Advanced Linux Sound Architecture Driver Initialized.
[ 0.282345] clocksource: Switched to clocksource timer1
[ 0.291540] NET: Registered protocol family 2
[ 0.292218] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.292264] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.292301] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.292430] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.292446] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.292588] NET: Registered protocol family 1
[ 0.292950] RPC: Registered named UNIX socket transport module.
[ 0.292964] RPC: Registered udp transport module.
[ 0.292969] RPC: Registered tcp transport module.
[ 0.292974] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.293816] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.295525] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.302316] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.303189] NFS: Registering the id_resolver key type
[ 0.303257] Key type id_resolver registered
[ 0.303265] Key type id_legacy registered
[ 0.303340] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.306513] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.306539] io scheduler noop registered
[ 0.306550] io scheduler deadline registered
[ 0.306688] io scheduler cfq registered (default)
[ 0.307880] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.311160] backlight supply power not found, using dummy regulator
[ 0.311405] pwm-backlight backlight: invalid default brightness level: 101, using 100
[ 0.362573] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.366160] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.000289] console [ttyS0] enabled
[ 1.004758] [drm] Initialized drm 1.1.0 20060810
[ 1.010353] panel panel: found backlight
[ 1.014419] ******************INIT**************
[ 1.019341] ******************PROBE**************
[ 1.025175] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.031829] [drm] No driver support for vblank timestamp query.
[ 1.070581] Console: switching to colour frame buffer device 128x37
[ 1.083285] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.112518] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.124533] loop: module loaded
[ 1.129787] libphy: Fixed MDIO Bus: probed
[ 1.192380] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.198520] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 1.205512] libphy: 4a101000.mdio: probed
[ 1.209552] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 1.219467] cpsw 4a100000.ethernet: Detected MACID = 04:a3:16:f8:0e:5c
[ 1.226257] cpsw 4a100000.ethernet: cpts: overflow check period 850
[ 1.234292] mousedev: PS/2 mouse device common for all mice
[ 1.240695] i2c /dev entries driver
[ 1.245273] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.252794] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.327621] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.337177] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.343409] mmc0: new SDHC card at address 0001
[ 1.350891] mmcblk0: mmc0:0001 uSD 3.72 GiB
[ 1.356541] NET: Registered protocol family 10
[ 1.363124] sit: IPv6 over IPv4 tunneling driver
[ 1.367929] mmcblk0: p1 p2
[ 1.371820] NET: Registered protocol family 17
[ 1.377328] Key type dns_resolver registered
[ 1.385015] omap_voltage_late_init: Voltage driver support not added
[ 1.419594] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 1.425289] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.432268] mmc1: MAN_BKOPS_EN bit is not set
[ 1.436810] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.443764] -----------------probing for EDT FT5x06 I2C-------------------
[ 1.456962] mmc1: new high speed MMC card at address 0001
[ 1.463261] mmcblk1: mmc1:0001 S10004 3.56 GiB
[ 1.468244] mmcblk1boot0: mmc1:0001 S10004 partition 1 4.00 MiB
[ 1.475094] input: EP0790M09 as /devices/platform/ocp/4802a000.i2c/i2c-1/1-0038/input/input0
[ 1.483650] mmcblk1boot1: mmc1:0001 S10004 partition 2 4.00 MiB
[ 1.490692] mmcblk1: p1
[ 1.493457] ------EDT FT5x06 initialized: IRQ 77, WAKE pin -1, Reset pin -1.
[ 1.501046] 1-001b supply IOVDD not found, using dummy regulator
[ 1.508746] 1-001b supply DVDD not found, using dummy regulator
[ 1.514870] 1-001b supply AVDD not found, using dummy regulator
[ 1.520849] 1-001b supply DRVDD not found, using dummy regulator
[ 1.527274] rtc-pcf8563 1-0051: chip found, driver version 0.4.4
[ 1.535452] rtc-pcf8563 1-0051: rtc core: registered rtc-pcf8563 as rtc0
[ 1.542582] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 1.549483] at24 2-0054: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.556658] at24 2-0055: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.563747] at24 2-0056: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.570851] at24 2-0057: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.577803] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 1.585895] rtc-pcf8563 1-0051: setting system clock to 2017-05-16 15:04:18 UTC (1494947058)
[ 1.598098] ALSA device list:
[ 1.601099] No soundcards found.
[ 1.627245] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 1.635580] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 1.645600] devtmpfs: mounted
[ 1.648939] Freeing unused kernel memory: 272K (c08d6000 - c091a000)
[ 1.655356] This architecture does not have kernel memory protection.
[ 2.303786] random: systemd: uninitialized urandom read (16 bytes read, 19 bits of entropy available)
[ 2.324689] random: systemd: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 2.361380] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 2.381300] systemd[1]: Detected architecture arm.
Welcome to [1mArago 2016.12[0m!
[ 2.415076] systemd[1]: Set hostname to <am335x-evm>.
[ 2.555610] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 2.567639] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 2.585180] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 2.623283] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 2.646634] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 26 bits of entropy available)
[ 2.796776] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 2.808119] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 2.819203] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 3.275314] systemd[1]: [/lib/systemd/system/gadget-init.service:15] Unknown lvalue 'ExecStopPre' in section 'Service'
[ 3.616859] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
[ 3.624846] systemd[1]: sysinit.target: Found dependency on alignment.service/start
[ 3.632808] systemd[1]: sysinit.target: Found dependency on basic.target/start
[ 3.640086] systemd[1]: sysinit.target: Found dependency on sockets.target/start
[ 3.647566] systemd[1]: sysinit.target: Found dependency on dbus.socket/start
[ 3.654808] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
[ 3.662258] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
[ 3.671761] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
[[0;1;31m SKIP [0m] Ordering cycle found, skipping alignment.service
[ 3.709838] systemd[1]: Listening on Journal Socket.
[[0;32m OK [0m] Listening on Journal Socket.
[ 3.733192] systemd[1]: Listening on udev Control Socket.
[[0;32m OK [0m] Listening on udev Control Socket.
[ 3.763443] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[[0;32m OK [0m] Started Dispatch Password Requests to Console Directory Watch.
[ 3.795117] systemd[1]: Created slice System Slice.
[[0;32m OK [0m] Created slice System Slice.
[ 3.827210] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 3.868218] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 3.918100] systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
[ 3.991175] systemd[1]: Listening on Network Service Netlink Socket.
[[0;32m OK [0m] Listening on Network Service Netlink Socket.
[ 4.023848] systemd[1]: Listening on Journal Socket (/dev/log).
[[0;32m OK [0m] Listening on Journal Socket (/dev/log).
[ 4.053007] systemd[1]: Listening on udev Kernel Socket.
[[0;32m OK [0m] Listening on udev Kernel Socket.
[ 4.084257] systemd[1]: Created slice User and Session Slice.
[[0;32m OK [0m] Created slice User and Session Slice.
[ 4.112816] systemd[1]: Reached target Slices.
[[0;32m OK [0m] Reached target Slices.
[ 4.137617] systemd[1]: Mounting Debug File System...
Mounting Debug File System...
[ 4.173052] systemd[1]: Reached target Remote File Systems.
[[0;32m OK [0m] Reached target Remote File Systems.
[ 4.202835] systemd[1]: Reached target Swap.
[[0;32m OK [0m] Reached target Swap.
[ 4.223177] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[[0;32m OK [0m] Started Forward Password Requests to Wall Directory Watch.
[ 4.252775] systemd[1]: Reached target Paths.
[[0;32m OK [0m] Reached target Paths.
[ 4.282967] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.319713] systemd[1]: Mounting Temporary Directory...
Mounting Temporary Directory...
[ 4.383281] systemd[1]: Listening on Syslog Socket.
[[0;32m OK [0m] Listening on Syslog Socket.
[ 4.418295] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.453434] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[[0;32m OK [0m] Listening on /dev/initctl Compatibility Named Pipe.
[ 4.493153] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.550879] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 4.559525] systemd[1]: Created slice system-serial\x2dgetty.slice.
[[0;32m OK [0m] Created slice system-serial\x2dgetty.slice.
[ 4.624242] systemd[1]: Created slice system-getty.slice.
[[0;32m OK [0m] Created slice system-getty.slice.
[ 4.694899] systemd[1]: Mounted POSIX Message Queue File System.
[[0;32m OK [0m] Mounted POSIX Message Queue File System.
[ 4.723086] systemd[1]: Mounted Debug File System.
[[0;32m OK [0m] Mounted Debug File System.
[ 4.736689] systemd[1]: Mounted Temporary Directory.
[[0;32m OK [0m] Mounted Temporary Directory.
[ 4.773559] systemd[1]: Started Journal Service.
[[0;32m OK [0m] Started Journal Service.
[[0;32m OK [0m] Started Setup Virtual Console.
[[0;32m OK [0m] Started Create list of required sta...ce nodes for the current kernel.
[[0;1;31mFAILED[0m] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[[0;32m OK [0m] Started Remount Root and Kernel File Systems.
Starting udev Coldplug all Devices...
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[[0;32m OK [0m] Started Apply Kernel Variables.
[[0;32m OK [0m] Started Create Static Device Nodes in /dev.
[ 6.206986] systemd-journald[100]: Received request to flush runtime journal from PID 1
[[0;32m OK [0m] Started Flush Journal to Persistent Storage.
[[0;32m OK [0m] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
Starting udev Kernel Device Manager...
[[0;32m OK [0m] Mounted /var/volatile.
[[0;32m OK [0m] Mounted /media/ram.
[[0;32m OK [0m] Started udev Kernel Device Manager.
[[0;32m OK [0m] Started udev Coldplug all Devices.
[[0;32m OK [0m] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
Starting Load/Save Random Seed...
[ 7.695921] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 7.811512] omap_rtc 44e3e000.rtc: already running
[ 7.870685] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc1
[[0;32m OK [0m] Started Create Volatile Files and Directories.[ 7.934537] 47401300.usb-phy supply vcc not found, using dummy regulator
[[0;32m OK [0m] Started Load/Save Random Seed.
[[0;32m OK [0m] Found device /dev/ttyS0.[ 8.065235] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 8.305280] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 8.835314] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 9.147843] remoteproc0: wkup_m3 is available
[ 9.152333] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 9.238129] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 9.300862] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ 9.744114] remoteproc0: powering up wkup_m3
[ 9.749543] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217280
[[0;32m OK [0m] Created slice system-systemd\x2dbacklight.slice.
Starting Load/Save Screen Backlight...htness of backlight:backlight...
[ 9.941357] remoteproc0: remote processor wkup_m3 is now up
[ 9.941378] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 10.080359] ti-pruss 4a300000.pruss: creating PRU cores and other child platform devices
[ 10.164663] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 10.172259] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[[0;32m OK [0m] Started Network Time Synchronization.
[[0;32m OK [0m] Started Load/Save Screen Backlight Brightness of backlight:backlight.
[ 10.325247] asoc-simple-card sound: asoc_simple_card_dai_link_of: Can't find simple-audio-card,codec DT node
[ 10.444209] remoteproc1: 4a334000.pru0 is available
[ 10.449221] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 10.474893] asoc-simple-card sound: parse error -22
[ 10.479856] asoc-simple-card: probe of sound failed with error -22
[ 10.605904] PM: bootloader does not support rtc-only!
[ 10.652552] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 10.811559] remoteproc1: registered virtio0 (type 7)
[ 10.838089] pru-rproc 4a334000.pru0: PRU rproc node /ocp/pruss@4a300000/pru0@4a334000 probed successfully
[[0;32m OK [0m] Found device /dev/ttyS3.
[ 10.947818] remoteproc2: 4a338000.pru1 is available
[ 11.022572] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 11.031600] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 11.114433] EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)
[ 11.210183] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 11.274805] remoteproc2: registered virtio1 (type 7)
[ 11.279990] pru-rproc 4a338000.pru1: PRU rproc node /ocp/pruss@4a300000/pru1@4a338000 probed successfully
[ 12.051596] random: nonblocking pool is initialized
[[0;32m OK [0m] Started Update UTMP about System Boot/Shutdown.
[[0;32m OK [0m] Found device /dev/mmcblk0p1.
[ 13.600989] usbcore: registered new interface driver usbfs
[ 13.634464] usbcore: registered new interface driver hub
[ 13.669854] usbcore: registered new device driver usb
[ 13.819266] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 13.902819] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1
[ 13.952844] remoteproc1: powering up 4a334000.pru0
[ 13.958266] remoteproc1: Booting fw image am335x-pru0-fw, size 75724
[ 13.973640] hub 1-0:1.0: USB hub found
[ 13.984039] hub 1-0:1.0: 1 port detected
[ 14.002838] ti-pruss 4a300000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[ 14.047437] remoteproc1: remote processor 4a334000.pru0 is now up
[ 14.073038] virtio_rpmsg_bus virtio0: creating channel rpmsg-pru addr 0x1e
[ 14.083879] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 14.123048] remoteproc2: powering up 4a338000.pru1
[ 14.128449] remoteproc2: Booting fw image am335x-pru1-fw, size 75724
[ 14.152703] ti-pruss 4a300000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[ 14.195964] remoteproc2: remote processor 4a338000.pru1 is now up
[ 14.209011] virtio_rpmsg_bus virtio1: creating channel rpmsg-pru addr 0x1f
[ 14.216895] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 14.280063] rpmsg_pru rpmsg0: new rpmsg_pru device: /dev/rpmsg_pru30
[ 14.298443] rpmsg_pru rpmsg1: new rpmsg_pru device: /dev/rpmsg_pru31
[[0;32m OK [0m] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
Starting Synchronize System and HW clocks...
[[0;32m OK [0m] Reached target System Time Synchronized.
[[0;32m OK [0m] Started Synchronize System and HW clocks.
[[0;32m OK [0m] Reached target System Initialization.
[[0;32m OK [0m] Started Daily Cleanup of Temporary Directories.
[[0;32m OK [0m] Reached target Timers.
[[0;32m OK [0m] Listening on RPCbind Server Activation Socket.
[[0;32m OK [0m] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[[0;32m OK [0m] Listening on dropbear.socket.
[[0;32m OK [0m] Listening on D-Bus System Message Bus Socket.
[[0;32m OK [0m] Reached target Sockets.
[[0;32m OK [0m] Reached target Basic System.
[[0;32m OK [0m] Started Kernel Logging Service.
Starting Avahi mDNS/DNS-SD Stack...
Starting Permit User Sessions...
Starting Print notice about GPLv3 packages...
Starting Login Service...
[[0;32m OK [0m] Started System Logging Service.
[[0;32m OK [0m] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
[[0;32m OK [0m] Started D-Bus System Message Bus.
[[0;32m OK [0m] Started Avahi mDNS/DNS-SD Stack.
Starting Network Service...
Starting Start USB gadget...
Starting Telephony service...
Starting uim-sysfs.service...
[[0;32m OK [0m] Started Permit User Sessions.
[ 16.032699] NET: Registered protocol family 15
[[0;32m OK [0m] Started Network Service.
[ 16.421360] net eth0: initializing cpsw version 1.12 (0)
[ 16.490858] net eth0: initialized cpsw ale version 1.4
[ 16.540008] net eth0: ALE Table size 1024
[ 16.561645] Bluetooth: Core ver 2.21
[ 16.601530] net eth0: phy found : id is : 0x7c0f1
[ 16.626301] NET: Registered protocol family 31
[ 16.659847] using random self ethernet address
[ 16.677185] using random host ethernet address
[ 16.681690] using host ethernet address: 04:A3:16:F8:0E:5E
[ 16.693303] Bluetooth: HCI device and connection manager initialized
[ 16.705158] libphy: PHY 4a101000.mdio:01 not found
[ 16.743245] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[ 16.757831] Bluetooth: HCI socket layer initialized
[ 16.777478] using random self ethernet address
[ 16.809872] Bluetooth: L2CAP socket layer initialized
[ 16.828245] using random host ethernet address
[ 16.852865] Bluetooth: SCO socket layer initialized
[ 16.875306] using host ethernet address: 04:A3:16:F8:0E:5E
[ 16.880818] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 16.930750] usb0: HOST MAC 04:a3:16:f8:0e:5e
[ 16.942047] Initializing XFRM netlink socket
[ 16.985506] usb0: MAC a6:c5:14:0b:61:c7
[ 17.084615] Mass Storage Function, version: 2009/09/11
[ 17.089842] LUN: removable file: (no medium)
[ 17.156608] LUN: removable read only file: /dev/mmcblk0p1
[ 17.218589] Number of LUNs=1
[ 17.248063] g_multi gadget: Multifunction Composite Gadget
[ 17.297050] g_multi gadget: g_multi ready
[[0;32m OK [0m] Found device /dev/ttyGS0.
[ 17.351128] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready
[ 17.725081] g_multi gadget: high-speed config #2: Multifunction with CDC ECM
[ 17.733020] IPv6: ADDRCONF(NETDEV_CHANGE): usb0: link becomes ready
[[0;32m OK [0m] Started Start USB gadget.
[[0;32m OK [0m] Started Telephony service.
[[0;32m OK [0m] Started Login Service.
Mounting Configuration File System...
[[0;32m OK [0m] Reached target Network.
Starting Lightning Fast Webserver With Light System Requirements...
Starting Network Name Resolution...
[[0;32m OK [0m] Started Serial Getty on ttyS3.
[[0;32m OK [0m] Started Getty on tty1.
[[0;32m OK [0m] Started Serial Getty on ttyS0.
[[0;32m OK [0m] Started Serial Getty on ttyGS0.
[[0;32m OK [0m] Mounted Configuration File System.
[[0;32m OK [0m] Started Network Name Resolution.
[[0;32m OK [0m] Started Lightning Fast Webserver With Light System Requirements.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
binutils
bison-dev
bison
cpp-symlinks
cpp
dosfstools
g++-symlinks
g++
gawk-dev
gawk
gcc-symlinks
gcc
gdb
gdbserver
gstreamer1.0-libav
hidapi
libcairo-perf-utils
libgmp10
libidn11
libmpc3
libmpfr4
m4-dev
m4
make
nettle
swig-dev
swig
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[[0;32m OK [0m] Started uim-sysfs.service.
[[0;32m OK [0m] Started Print notice about GPLv3 packages.
Starting telnetd.service...
[[0;32m OK [0m] Started telnetd.service.
Starting busybox-udhcpd.service...
Starting thttpd.service...
[[0;32m OK [0m] Started busybox-udhcpd.service.
[[0;32m OK [0m] Started thttpd.service.
Starting rng-tools.service...
[[0;32m OK [0m] Started rng-tools.service.
Starting matrix-gui-2.0.service...
[[0;32m OK [0m] Started matrix-gui-2.0.service.
Starting thermal-zone-init.service...
Starting parse-ip.service...
[[0;32m OK [0m] Started thermal-zone-init.service.
[[0;32m OK [0m] Started parse-ip.service.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS0
Arago 2016.12 am335x-evm ttyS0
am335x-evm login: [ 47.238217] edt_ft5x06 1-0038: Unable to fetch data, error: -121
[ 54.432685] usb 1-1: new low-speed USB device number 2 using musb-hdrc
[ 54.812761] input: PixArt USB Optical Mouse as /devices/platform/ocp/47400000.usb/47401c00.usb/musb-hdrc.1.auto/usb1/1-1/1-1:1.0/0003:093A:2510.0001/input/input1
[ 54.831737] hid-generic 0003:093A:2510.0001: input: USB HID v1.11 Mouse [PixArt USB Optical Mouse] on usb-musb-hdrc.1.auto-1/input0
[ 54.851794] usbcore: registered new interface driver usbhid
[ 54.861952] usbhid: USB HID core driver
[ 210.673170] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 210.717752] nf_conntrack version 0.5.0 (7958 buckets, 31832 max)
Please find the Dmesg log.
root@am335x-evm:~# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.41-gf9f6f0db2d (root@fg-1) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #11 PREEMPT Wed May 17 19:02:29 IST 2017
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x BeagleBone Black
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] On node 0 totalpages: 131072
[ 0.000000] free_area_init_node: node 0, pgdat c09691d4, node_mem_map dcb61000
[ 0.000000] Normal zone: 1152 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 131072 pages, LIFO batch:31
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=000c50d8-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 459912K/524288K available (6627K kernel code, 325K rwdata, 2384K rodata, 272K init, 265K bss, 15224K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0xc0008000 - 0xc08d5004 (9013 kB)
.init : 0xc08d6000 - 0xc091a000 ( 272 kB)
.data : 0xc091a000 - 0xc096b630 ( 326 kB)
.bss : 0xc096b630 - 0xc09add58 ( 266 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000013] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000032] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000040] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000188] clocksource_probe: no matching clocksources found
[ 0.000339] Console: colour dummy device 80x30
[ 0.000362] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000368] This ensures that you still see kernel messages. Please
[ 0.000372] update your kernel commandline.
[ 0.000388] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736)
[ 0.089233] pid_max: default: 32768 minimum: 301
[ 0.089348] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089358] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.089962] Initializing cgroup subsys io
[ 0.089990] Initializing cgroup subsys memory
[ 0.090025] Initializing cgroup subsys devices
[ 0.090038] Initializing cgroup subsys freezer
[ 0.090050] Initializing cgroup subsys perf_event
[ 0.090060] Initializing cgroup subsys pids
[ 0.090084] CPU: Testing write buffer coherency: ok
[ 0.090446] Setting up static identity map for 0x80008200 - 0x80008260
[ 0.092248] devtmpfs: initialized
[ 0.102655] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.115464] omap_hwmod: debugss: _wait_target_disable failed
[ 0.170926] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.174414] pinctrl core: initialized pinctrl subsystem
[ 0.175589] NET: Registered protocol family 16
[ 0.177419] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.199227] cpuidle: using governor ladder
[ 0.229215] cpuidle: using governor menu
[ 0.232748] gpiochip_add: registered GPIOs 0 to 31 on device: gpio
[ 0.233021] OMAP GPIO hardware version 0.1
[ 0.233699] gpiochip_add: registered GPIOs 32 to 63 on device: gpio
[ 0.234366] gpiochip_add: registered GPIOs 64 to 95 on device: gpio
[ 0.235001] gpiochip_add: registered GPIOs 96 to 127 on device: gpio
[ 0.242159] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.276260] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.276593] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/fixedregulator@0[0]'
[ 0.279609] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.279663] omap_i2c 4802a000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c1_pins, deferring probe
[ 0.279694] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe
[ 0.279815] media: Linux media interface: v0.10
[ 0.279863] Linux video capture interface: v2.00
[ 0.279903] pps_core: LinuxPPS API ver. 1 registered
[ 0.279909] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.279953] PTP clock support registered
[ 0.280001] EDAC MC: Ver: 3.0.0
[ 0.281001] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.281306] Advanced Linux Sound Architecture Driver Initialized.
[ 0.282346] clocksource: Switched to clocksource timer1
[ 0.291535] NET: Registered protocol family 2
[ 0.292208] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.292254] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.292291] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.292417] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.292434] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.292574] NET: Registered protocol family 1
[ 0.292936] RPC: Registered named UNIX socket transport module.
[ 0.292949] RPC: Registered udp transport module.
[ 0.292955] RPC: Registered tcp transport module.
[ 0.292960] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.292982] PCI: CLS 0 bytes, default 64
[ 0.293808] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.295517] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.302311] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.303183] NFS: Registering the id_resolver key type
[ 0.303250] Key type id_resolver registered
[ 0.303258] Key type id_legacy registered
[ 0.303333] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.306501] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.306529] io scheduler noop registered
[ 0.306539] io scheduler deadline registered
[ 0.306679] io scheduler cfq registered (default)
[ 0.307874] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.311083] pwm-backlight backlight: GPIO lookup for consumer enable
[ 0.311105] pwm-backlight backlight: using device tree for GPIO lookup
[ 0.311118] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/backlight[0]'
[ 0.311127] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/backlight[0]'
[ 0.311136] pwm-backlight backlight: using lookup tables for GPIO lookup
[ 0.311145] pwm-backlight backlight: lookup for GPIO enable failed
[ 0.311165] backlight supply power not found, using dummy regulator
[ 0.311416] pwm-backlight backlight: invalid default brightness level: 101, using 100
[ 0.362550] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.366141] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.000271] console [ttyS0] enabled
[ 1.004748] [drm] Initialized drm 1.1.0 20060810
[ 1.010350] panel panel: found backlight
[ 1.014360] panel panel: GPIO lookup for consumer enable
[ 1.014369] panel panel: using device tree for GPIO lookup
[ 1.014381] of_get_named_gpiod_flags: can't parse 'enable-gpios' property of node '/panel[0]'
[ 1.014390] of_get_named_gpiod_flags: can't parse 'enable-gpio' property of node '/panel[0]'
[ 1.014398] panel panel: using lookup tables for GPIO lookup
[ 1.014407] panel panel: lookup for GPIO enable failed
[ 1.014414] ******************INIT**************
[ 1.019339] ******************PROBE**************
[ 1.025174] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.031823] [drm] No driver support for vblank timestamp query.
[ 1.070563] Console: switching to colour frame buffer device 128x37
[ 1.083261] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.112514] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.124534] loop: module loaded
[ 1.129783] libphy: Fixed MDIO Bus: probed
[ 1.192382] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.198522] davinci_mdio 4a101000.mdio: detected phy mask fffffffe
[ 1.205490] libphy: 4a101000.mdio: probed
[ 1.209529] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720
[ 1.219441] cpsw 4a100000.ethernet: Detected MACID = 04:a3:16:f8:0e:5c
[ 1.226232] cpsw 4a100000.ethernet: cpts: overflow check period 850
[ 1.234267] mousedev: PS/2 mouse device common for all mice
[ 1.240666] i2c /dev entries driver
[ 1.245236] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.252641] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 1.252656] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.252684] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@48060000[0]' - status (0)
[ 1.252761] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.257406] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[ 1.257414] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.257423] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@48060000[0]'
[ 1.257432] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@48060000[0]'
[ 1.257440] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[ 1.257449] omap_hsmmc 48060000.mmc: lookup for GPIO wp failed
[ 1.292865] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
[ 1.292885] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.292897] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@481d8000[0]'
[ 1.292907] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@481d8000[0]'
[ 1.292916] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 1.292924] omap_hsmmc 481d8000.mmc: lookup for GPIO cd failed
[ 1.293017] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
[ 1.293028] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.293037] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@481d8000[0]'
[ 1.293044] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@481d8000[0]'
[ 1.293052] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 1.293060] omap_hsmmc 481d8000.mmc: lookup for GPIO wp failed
[ 1.327622] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.336294] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@2[0]' - status (0)
[ 1.336511] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@3[0]' - status (0)
[ 1.336650] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@4[0]' - status (0)
[ 1.336755] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds/led@5[0]' - status (0)
[ 1.337190] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.343418] mmc0: new SDHC card at address 0001
[ 1.350903] mmcblk0: mmc0:0001 uSD 3.72 GiB
[ 1.356552] NET: Registered protocol family 10
[ 1.363167] mmcblk0: p1 p2
[ 1.366331] sit: IPv6 over IPv4 tunneling driver
[ 1.371674] NET: Registered protocol family 17
[ 1.377382] Key type dns_resolver registered
[ 1.385079] omap_voltage_late_init: Voltage driver support not added
[ 1.419569] tps65217 0-0024: TPS65217 ID 0xe version 1.2
[ 1.425260] at24 0-0050: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.432202] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.439290] -----------------probing for EDT FT5x06 I2C-------------------
[ 1.446322] edt_ft5x06 1-0038: GPIO lookup for consumer reset
[ 1.446334] edt_ft5x06 1-0038: using device tree for GPIO lookup
[ 1.446347] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/i2c@4802a000/edt-ft5x06@38[0]'
[ 1.446356] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/i2c@4802a000/edt-ft5x06@38[0]'
[ 1.446364] edt_ft5x06 1-0038: using lookup tables for GPIO lookup
[ 1.446373] edt_ft5x06 1-0038: lookup for GPIO reset failed
[ 1.446382] edt_ft5x06 1-0038: GPIO lookup for consumer wake
[ 1.446388] edt_ft5x06 1-0038: using device tree for GPIO lookup
[ 1.446396] of_get_named_gpiod_flags: can't parse 'wake-gpios' property of node '/ocp/i2c@4802a000/edt-ft5x06@38[0]'
[ 1.446404] of_get_named_gpiod_flags: can't parse 'wake-gpio' property of node '/ocp/i2c@4802a000/edt-ft5x06@38[0]'
[ 1.446411] edt_ft5x06 1-0038: using lookup tables for GPIO lookup
[ 1.446418] edt_ft5x06 1-0038: lookup for GPIO wake failed
[ 1.459306] mmc1: MAN_BKOPS_EN bit is not set
[ 1.465869] input: EP0790M09 as /devices/platform/ocp/4802a000.i2c/i2c-1/1-0038/input/input0
[ 1.475030] ------EDT FT5x06 initialized: IRQ 77, WAKE pin -1, Reset pin -1.
[ 1.482660] of_get_named_gpiod_flags: can't parse 'gpio-reset' property of node '/ocp/i2c@4802a000/tlv320aic3x@1b[0]'
[ 1.482699] 1-001b supply IOVDD not found, using dummy regulator
[ 1.488875] 1-001b supply DVDD not found, using dummy regulator
[ 1.494945] mmc1: new high speed MMC card at address 0001
[ 1.500714] 1-001b supply AVDD not found, using dummy regulator
[ 1.506993] mmcblk1: mmc1:0001 S10004 3.56 GiB
[ 1.511660] 1-001b supply DRVDD not found, using dummy regulator
[ 1.517985] mmcblk1boot0: mmc1:0001 S10004 partition 1 4.00 MiB
[ 1.524309] rtc-pcf8563 1-0051: pcf8563_probe
[ 1.524324] rtc-pcf8563 1-0051: chip found, driver version 0.4.4
[ 1.530665] mmcblk1boot1: mmc1:0001 S10004 partition 2 4.00 MiB
[ 1.537318] rtc-pcf8563 1-0051: low voltage detected, date/time is not reliable.
[ 1.545072] rtc rtc0: read_time: fail to read: -22
[ 1.545293] rtc rtc0: rtc-pcf8563: dev (254:0)
[ 1.545322] rtc-pcf8563 1-0051: rtc core: registered rtc-pcf8563 as rtc0
[ 1.552209] mmcblk1: p1
[ 1.555995] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 400 kHz
[ 1.563651] at24 2-0054: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.570841] at24 2-0055: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.578027] at24 2-0056: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.585146] at24 2-0057: 32768 byte 24c256 EEPROM, writable, 1 bytes/write
[ 1.592108] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz
[ 1.600160] rtc-pcf8563 1-0051: low voltage detected, date/time is not reliable.
[ 1.607727] rtc rtc0: read_time: fail to read: -22
[ 1.607738] rtc-pcf8563 1-0051: hctosys: unable to read the hardware clock
[ 1.618271] ALSA device list:
[ 1.621274] No soundcards found.
[ 1.649447] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 1.657811] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 1.667661] devtmpfs: mounted
[ 1.670951] Freeing unused kernel memory: 272K (c08d6000 - c091a000)
[ 1.677368] This architecture does not have kernel memory protection.
[ 2.214951] systemd[1]: System time before build time, advancing clock.
[ 2.332957] random: systemd: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 2.353637] random: systemd: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
[ 2.390386] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
[ 2.410270] systemd[1]: Detected architecture arm.
[ 2.445218] systemd[1]: Set hostname to <am335x-evm>.
[ 2.578636] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 2.591079] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 23 bits of entropy available)
[ 2.614448] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 24 bits of entropy available)
[ 2.649396] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 25 bits of entropy available)
[ 2.673296] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 26 bits of entropy available)
[ 2.823819] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 2.834012] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 2.844997] random: systemd: uninitialized urandom read (16 bytes read, 30 bits of entropy available)
[ 3.299723] systemd[1]: [/lib/systemd/system/gadget-init.service:15] Unknown lvalue 'ExecStopPre' in section 'Service'
[ 3.644074] systemd[1]: sockets.target: Found ordering cycle on sockets.target/start
[ 3.652010] systemd[1]: sockets.target: Found dependency on rpcbind.socket/start
[ 3.659574] systemd[1]: sockets.target: Found dependency on sysinit.target/start
[ 3.667119] systemd[1]: sockets.target: Found dependency on alignment.service/start
[ 3.674890] systemd[1]: sockets.target: Found dependency on basic.target/start
[ 3.682161] systemd[1]: sockets.target: Found dependency on sockets.target/start
[ 3.689656] systemd[1]: sockets.target: Breaking ordering cycle by deleting job rpcbind.socket/start
[ 3.698870] systemd[1]: rpcbind.socket: Job rpcbind.socket/start deleted to break ordering cycle starting with sockets.target/start
[ 3.734237] systemd[1]: alignment.service: Found ordering cycle on alignment.service/start
[ 3.742720] systemd[1]: alignment.service: Found dependency on sysinit.target/start
[ 3.750484] systemd[1]: alignment.service: Found dependency on alignment.service/start
[ 3.758512] systemd[1]: alignment.service: Breaking ordering cycle by deleting job alignment.service/start
[ 3.768285] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with alignment.service/start
[ 3.808763] systemd[1]: Listening on Journal Socket (/dev/log).
[ 3.832905] systemd[1]: Reached target Remote File Systems.
[ 3.862705] systemd[1]: Reached target Swap.
[ 3.882945] systemd[1]: Listening on udev Kernel Socket.
[ 3.915289] systemd[1]: Created slice User and Session Slice.
[ 3.943179] systemd[1]: Listening on Journal Socket.
[ 3.974170] systemd[1]: Created slice System Slice.
[ 4.007222] systemd[1]: Starting Remount Root and Kernel File Systems...
[ 4.044927] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 4.118664] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 4.128500] systemd[1]: Starting Setup Virtual Console...
[ 4.199012] systemd[1]: Starting Create list of required static device nodes for the current kernel...
[ 4.268258] systemd[1]: Mounting POSIX Message Queue File System...
[ 4.324659] systemd[1]: Created slice system-getty.slice.
[ 4.352831] systemd[1]: Reached target Slices.
[ 4.373016] systemd[1]: Listening on Syslog Socket.
[ 4.407246] systemd[1]: Mounting Debug File System...
[ 4.443385] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ 4.473478] systemd[1]: Listening on Network Service Netlink Socket.
[ 4.503199] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 4.532741] systemd[1]: Reached target Paths.
[ 4.565545] systemd[1]: Starting Journal Service...
[ 4.603230] systemd[1]: Listening on udev Control Socket.
[ 4.655364] systemd[1]: Mounting Temporary Directory...
[ 4.720227] systemd[1]: Starting Load Kernel Modules...
[ 4.763457] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 4.859477] systemd[1]: Mounted POSIX Message Queue File System.
[ 4.903228] systemd[1]: Mounted Debug File System.
[ 4.923248] systemd[1]: Mounted Temporary Directory.
[ 4.953596] systemd[1]: Started Journal Service.
[ 6.330456] systemd-journald[102]: Received request to flush runtime journal from PID 1
[ 7.742601] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 7.827025] rtc rtc1: 44e3e000.rtc: dev (254:1)
[ 7.827055] omap_rtc 44e3e000.rtc: rtc core: registered 44e3e000.rtc as rtc1
[ 7.907222] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer reset
[ 7.907252] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[ 7.907267] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 7.907276] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 7.907285] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[ 7.907295] am335x-phy-driver 47401300.usb-phy: lookup for GPIO reset failed
[ 7.907305] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer vbus-detect
[ 7.907313] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[ 7.907321] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 7.907329] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 7.907336] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[ 7.907345] am335x-phy-driver 47401300.usb-phy: lookup for GPIO vbus-detect failed
[ 7.907408] 47401300.usb-phy supply vcc not found, using dummy regulator
[ 8.004545] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer reset
[ 8.004574] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[ 8.004590] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 8.004599] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 8.004607] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[ 8.004617] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO reset failed
[ 8.004626] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer vbus-detect
[ 8.004634] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[ 8.004643] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 8.004651] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 8.004658] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[ 8.004666] am335x-phy-driver 47401b00.usb-phy: lookup for GPIO vbus-detect failed
[ 8.004730] 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 8.523937] omap_rng 48310000.rng: OMAP Random Number Generator ver. 20
[ 8.976499] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 9.236401] remoteproc0: wkup_m3 is available
[ 9.240890] remoteproc0: Note: remoteproc is still under development and considered experimental.
[ 9.394250] remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 9.702297] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 9.883615] remoteproc0: powering up wkup_m3
[ 9.929557] remoteproc0: Booting fw image am335x-pm-firmware.elf, size 217280
[ 10.033257] remoteproc0: remote processor wkup_m3 is now up
[ 10.033275] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 10.082683] ti-pruss 4a300000.pruss: creating PRU cores and other child platform devices
[ 10.091972] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 10.267952] irq: no irq domain found for /ocp/pruss@4a300000/intc@4a320000 !
[ 10.289560] asoc-simple-card sound: asoc_simple_card_dai_link_of: Can't find simple-audio-card,codec DT node
[ 10.416055] remoteproc1: 4a334000.pru0 is available
[ 10.421067] remoteproc1: Note: remoteproc is still under development and considered experimental.
[ 10.430837] asoc-simple-card sound: parse error -22
[ 10.468432] asoc-simple-card: probe of sound failed with error -22
[ 10.538485] PM: bootloader does not support rtc-only!
[ 10.598161] remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 10.757701] remoteproc1: registered virtio0 (type 7)
[ 10.810951] pru-rproc 4a334000.pru0: PRU rproc node /ocp/pruss@4a300000/pru0@4a334000 probed successfully
[ 10.916490] remoteproc2: 4a338000.pru1 is available
[ 10.921505] remoteproc2: Note: remoteproc is still under development and considered experimental.
[ 11.137770] remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
[ 11.170222] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 11.240447] remoteproc2: registered virtio1 (type 7)
[ 11.280067] pru-rproc 4a338000.pru1: PRU rproc node /ocp/pruss@4a300000/pru1@4a338000 probed successfully
[ 11.535668] EXT4-fs (mmcblk1p1): recovery complete
[ 11.562532] EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)
[ 12.431753] random: nonblocking pool is initialized
[ 13.630171] usbcore: registered new interface driver usbfs
[ 13.700326] usbcore: registered new interface driver hub
[ 13.742786] usbcore: registered new device driver usb
[ 13.836704] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 13.836731] musb-hdrc: MHDRC RTL version 2.0
[ 13.836739] musb-hdrc: setup fifo_mode 4
[ 13.836758] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 13.859280] musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
[ 13.859308] musb-hdrc: MHDRC RTL version 2.0
[ 13.859317] musb-hdrc: setup fifo_mode 4
[ 13.859333] musb-hdrc: 28/31 max ep, 16384/16384 memory
[ 13.859461] musb-hdrc musb-hdrc.1.auto: MUSB HDRC host driver
[ 13.928236] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 1
[ 13.998777] remoteproc1: powering up 4a334000.pru0
[ 14.004285] hub 1-0:1.0: USB hub found
[ 14.015310] hub 1-0:1.0: 1 port detected
[ 14.024237] remoteproc1: Booting fw image am335x-pru0-fw, size 75724
[ 14.042763] ti-pruss 4a300000.pruss: configured system_events = 0x0000000000030000 intr_channels = 0x00000005 host_intr = 0x00000005
[ 14.092645] remoteproc1: remote processor 4a334000.pru0 is now up
[ 14.116752] virtio_rpmsg_bus virtio0: creating channel rpmsg-pru addr 0x1e
[ 14.124655] virtio_rpmsg_bus virtio0: rpmsg host is online
[ 14.161672] remoteproc2: powering up 4a338000.pru1
[ 14.167515] remoteproc2: Booting fw image am335x-pru1-fw, size 75724
[ 14.195084] ti-pruss 4a300000.pruss: configured system_events = 0x00000000000c0000 intr_channels = 0x0000000a host_intr = 0x0000000a
[ 14.235527] remoteproc2: remote processor 4a338000.pru1 is now up
[ 14.246102] virtio_rpmsg_bus virtio1: creating channel rpmsg-pru addr 0x1f
[ 14.253921] virtio_rpmsg_bus virtio1: rpmsg host is online
[ 14.326579] rpmsg_pru rpmsg0: new rpmsg_pru device: /dev/rpmsg_pru30
[ 14.344991] rpmsg_pru rpmsg1: new rpmsg_pru device: /dev/rpmsg_pru31
[ 14.684134] rtc-pcf8563 1-0051: pcf8563_set_datetime: secs=17, mins=2, hours=15, mday=16, mon=4, year=117, wday=2
[ 14.688672] rtc-pcf8563 1-0051: pcf8563_get_datetime: raw data is st1=08, st2=00, sec=17, min=02, hr=15, mday=16, wday=12, mon=05, year=17
[ 14.688701] rtc-pcf8563 1-0051: pcf8563_get_datetime: tm is secs=17, mins=2, hours=15, mday=16, mon=4, year=117, wday=2
[ 14.688715] rtc-pcf8563 1-0051: pcf8563_irq_enable: en=0
[ 15.606352] using random self ethernet address
[ 15.610850] using random host ethernet address
[ 15.632908] NET: Registered protocol family 15
[ 15.661302] using host ethernet address: 04:A3:16:F8:0E:5E
[ 15.684266] using random self ethernet address
[ 15.705910] using random host ethernet address
[ 15.734031] using host ethernet address: 04:A3:16:F8:0E:5E
[ 15.776181] usb0: HOST MAC 04:a3:16:f8:0e:5e
[ 15.847494] usb0: MAC f2:7f:2e:67:68:31
[ 15.885013] Bluetooth: Core ver 2.21
[ 15.926897] NET: Registered protocol family 31
[ 15.960647] Mass Storage Function, version: 2009/09/11
[ 16.015601] Bluetooth: HCI device and connection manager initialized
[ 16.030426] LUN: removable file: (no medium)
[ 16.086997] LUN: removable read only file: /dev/mmcblk0p1
[ 16.113193] Bluetooth: HCI socket layer initialized
[ 16.180021] Number of LUNs=1
[ 16.191457] Bluetooth: L2CAP socket layer initialized
[ 16.227839] g_multi gadget: Multifunction Composite Gadget
[ 16.254700] Bluetooth: SCO socket layer initialized
[ 16.279129] g_multi gadget: g_multi ready
[ 16.562975] IPv6: ADDRCONF(NETDEV_UP): usb0: link is not ready
[ 16.580354] Initializing XFRM netlink socket
[ 16.812549] net eth0: initializing cpsw version 1.12 (0)
[ 16.843127] net eth0: initialized cpsw ale version 1.4
[ 16.886793] net eth0: ALE Table size 1024
[ 16.948311] net eth0: phy found : id is : 0x7c0f1
[ 16.980342] libphy: PHY 4a101000.mdio:01 not found
[ 17.022821] net eth0: phy "4a101000.mdio:01" not found on slave 1, err -19
[ 17.091996] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 41.300515] g_multi gadget: high-speed config #2: Multifunction with CDC ECM
[ 41.316192] hrtimer: interrupt took 249750 ns
[ 41.332741] IPv6: ADDRCONF(NETDEV_CHANGE): usb0: link becomes ready
2. Not able to run any of the video from matrix window(3D & other example video which is accessible from matrix).
Can you please let me know, do i need to enable some other graphic driver for this? Or do i need to use the graphic SDK instead of TI SDK which i'm using currently.
Replay ASAP.
Thanks,
Shekar