Part Number: AM5718
Other Parts Discussed in Thread: TMDXIDK5718, SYSBIOS
Hello,
we would like to implement a gateway using the PRU-ICSS-ETHERCAT-SLAVE (v1.00.02), as well as the PRU-ICSS-PROFINET-SLAVE (v1.00.00) kits from TI.
Our problem:
- PRU-ICSS-ETHERCAT-SLAVE -> It is recommended to use SDK 3.2.0, CCS 6.1.3, Compiler gcc-arm-none-eabi-4_9-2015q3
- PRU-ICSS-PROFINET-SLAVE -> It is recommended to use SDK 2.0.2, CCS 6.1.2, Compiler gcc-arm-none-eabi-4_8-2014q3
Which SDK/CCS/Compiler do we have to use now for the whole project?
At the moment we have installed
Processor SDK RTOS for AM57XX v3.3.0.4
CCS 7.0.0.00043
and we use the compiler Linaro 4.9
With this we are not able to put the system into operation.
Furthermore we tried some example projects. They always include a lot of stuff like LED switching, SD card access,... Do you also have a very simple project, which just illustrates the use of the protocol stacks?
Thank you
and best regards,
Manuel