Part Number: AM3352
Hello,
I have a very strange problem with a custom board. The board is very similar to beagle black with AM3352 and a single ddr3 memory. I have two identical verions of the board: one with micron MT41J128M16-125 and one with samsung K4B4G1646D-BCK0. I can't initialize the ddr3 correctly in both boards. After initialization, if I write 0xFFFFFFFF I read 0xDFFFDFFF and if I write 0xAA55AA55 I get 0x8A558A55. I have tried all the possible consigurations in u-boot SPL and in starterware in UART boot mode. It seems that the same bit in both byte lanes have problem. How is this possible? Does it look like a timming configuration problem, or a pcb trace routing problem?
I have read all the relative TI's support documents and I have used all the spreadsheet tools for calculating parameters.
Can anybody help me with this problem?
Thanks.