Dear:
Now I faced a strange problem. Simulation speed of running the program run much faster than offline. I use AISgen for D800k002 tools create. bin file, and then programmed to flash in spiflash_writer_dsp.pjt program. However, the power automatically load programs, running speed significantly slower . I do not know where the problem?
In AISgen for D800k002 ,Configuration is as follows:
In General,I choose SPI1 Flash, Crystal 24MHz,Configure PLL0,Configure PLL1,Configure DDR,Configure PSC.
In Peripheral, Module Clock 150 MHz,SPI Clock 1MHz.
In PLL0,parameters are 1,25,2,1,3,6
In PLL1,parameters are 11,2,1,2,3
In DDR, Memory Type is mDDR,DRPYC1R is 0x000000C4,SDCR is 0x0A034622,SDCR2 is 0x00000000,SDTIMR1 is 0x184929C8,SDTIMR2 is 0x380FC700,SDRCR is 0x00000406.
In PSC,PSC0 choose 0;1;2,PSC1 choose 3;5;10
Compile the program does not gel content!
please help me!
Thanks!