Part Number: BEAGLEBK
Other Parts Discussed in Thread: BEAGLEBOARD-X15
Where would I find an example of some simple image processing (CVBS camera input, some kind of kernel-based filtering, with the ouptut images saved to a bmp or a compressed file type, served up over a webserver running on the ARM code)? And will I have to build this under Linux, or will the latest Eclipse-based CCS7 do?
I wonder if the Sitara examples still use XDC, SYS BIOS, iALG, XDAIS or if these have been replaced by some equivalents. In which case, what are their names?
The camera could be a Webcam rather than a CVBS, but ultimately, I'm going to need something like the DaVinci's VPFE - is that present in the Sitara?